Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Includes or excludes the optional Release 98 Extension element from the Assistance Data component. You can set the value of these fields using the following commands: CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98:BTS[<n>]:EOTDiff CALL:PPRocedure:PMEasurement:MPRequest:REL98|RELEASE98:BTS[<n>]:EOTDiff:UNCertainty | |
EGPRS LA | ||
INCLude|EXCLude | ||
INCL|EXCL | ||
EXCL | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:ADATa:REL98 INCL" |