Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Queries to determine if the optional Multiple Sets element is included in the Measurement Position Response component from the MS. If this element is not included, none of the values in this element will be available. Therefore, CALL:PPRocedure:PMEasurement:PRESponse:MSETs:SETS:NUMBer? , CALL:PPRocedure:PMEasurement:PRESponse:MSETs:RBTS:NUMBer? , and CALL:PPRocedure:PMEasurement:PRESponse:MSETs:RBTS:RELation? will all return NAN (Not a number). | |
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:MSETS:INCLuded?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Queries the Number of Reference BTS field of the optional Multiple Sets element. If the Multiple Sets element is not included, values for this field will not be available. See CALL:PPRocedure:PMEasurement:PRESponse:MSETs:INCLuded? to determine if the element is included. | |
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:MSETS:RBTS:NUMBer?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Queries the Reference BTS Relation to Measurement Elements field of the optional Multiple Sets element. If the Multiple Sets element is not included, values for this field will not be available. See CALL:PPRocedure:PMEasurement:PRESponse:MSETs:INCLuded? to determine if the element is included. | |
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:MSETS:RBTS:RELation?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | Queries the Reference BTS Relation to Measurement Elements field of the optional Multiple Sets element. If the Multiple Sets element is not included, values for this field will not be available. See CALL:PPRocedure:PMEasurement:PRESponse:MSETs:INCLuded? to determine if the element is included. | |
EGPRS LA | ||
Query | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:PMEasurement:PRESponse:MSETS:SETS:NUMBer?" |