Last updated: December 3, 2008
This command is not applicable to the GSM test applications. | ||
GPRS TA | This command is not applicable to the GPRS test applications. | |
EGPRS TA | This command is not applicable to the EGPRS test applications. | |
GSM/GPRS LA |
This command sets the Routing Area Update Reject cause. See GMM Cause Information Element for details on settings this parameter accepts as defined in 3GPP TS 24.008 Version 6.7.0. |
|
EGPRS LA | ||
Setting | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPRocedure:RAUPdate:REJect:GMMCause 7" ! The test set sends the MS the RAU Reject cause value as "GPRS Services Not Allowed". |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets the Periodic Routing Update Timer value. See Configurable Timers . The size of the layer 3 message field is limited and to provide large range of values the following rounding will be applied to the actual value sent to the MS. |
|
EGPRS LA | ||
Setting | ||
0 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:PPROCEDURE:RAU:T3312 10" ! Set the expire time of T3312 to 10 seconds. |