Last updated: December 3, 2008
Function | GSM TA |
This command is not applicable to the GSM Test Applications. |
This command is not applicable to the GPRS Test Applications. |
||
This command is not applicable to the EGPRS Test Applications. |
||
This command sets/queries the Packet SI/PSI Status Indication State. When this parameter is set to ON, the test set will indicate the supporting of the packet SI/PSI Status message in the SI13 message (on BCCH) or PSI1 message (on PBCCH). The mobile can request the specific SI/PSI messages to be transferred from the test set when working in the Packet Transfer state; Upon receiving the SI/PSI request messages the test set provides the requested broadcast information messages over the available PACCH associated with an active TBF between the mobile and the test set. Note: The Operating Mode must be set to Cell Off before setting this parameter. See CALL:OPERating for more details. |
||
0|OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:CELL:PSINdication ON" ! Set the Packet (P)SI status Indication State to ON. |