Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This parameter sets the 128 bit random number used as a challenge to MS in an authentication request. See Random(RAND) Value for more information. |
|
EGPRS LA | ||
Range: 0 to FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF | ||
Range: "00000000:00000000:00000000:00000000" to "FFFFFFFF:FFFFFFFF:FFFFFFFF:FFFFFFFF" | ||
"00000000:00000000:00000000:00000000" | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:RANDom 'B'" ! Sets the random value of the Authentication Parameter to 00000000:00000000:00000000:0000000B. |
Function | This command is not applicable to the GSM Test Application. | |
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This parameter queries the Authentication Result for MM authentication procedure. See Authentication Result: MM (CS domain) for more information. | |
EGPRS LA | ||
Range: SUCCess|MSFAILUN|KNOWN|RESNOTMA|TCH|NULL | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:RESult?" ! Queries the MM authentication result. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | When this parameter is set to ON, the test set will perform an authentication challenge to the MS on every opportunity. This parameter sets Authentication State. See Authentication State for more information. | |
EGPRS LA | ||
Range: 1|ON|0|OFF | ||
Range: 1|0 | ||
0|OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:STATe ON" ! Sets Authentication state to ON. |
Function | This command is not applicable to the GSM Test Application. | |
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This parameter sets the 32 bit expected response used to compare with the actual SRES sent from the MS as a response to the RAND challenge. See XRES for more information. | |
EGPRS LA | ||
Range: 0 to FFFFFFFF | ||
Range: "00000000" to "FFFFFFFF" | ||
"00000000" | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SECurity:AUTHenticate:XRESult `E34B7AD8'" ! Sets the XRESult value of the Authentication Parameter to E34B7AD8. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This parameter sets the 64 bit number used as an entry parameter to the selected encryption algorithm. See Ciphering Key(Kc) for more information. | |
EGPRS LA | ||
Range: 0 to FFFFFFFFFFFFFFFF | ||
Range: "00000000:00000000" to "FFFFFFFF:FFFFFFFF" | ||
"0000000000000000" | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SECurity:Ciphering `7C'" ! Sets the ciphering key to 00000000:0000007C. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This parameter sets Cipher Key Sequence Number. See Cipher Key Sequence Number (CKSN) for more information. | |
EGPRS LA | ||
Range: 0 to 7 | ||
Range: 0 to 7 | ||
1 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SECurity:Ciphering:CKSNumber 1" ! Sets the CKSN to 1. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA | This parameter sets which ciphering algorithm will be used for GPRS packet switched data. See GPRS Ciphering Algorithm for more information. | |
EGPRS LA | ||
Range: OFF|GEA1|GEA2|GEA3 | ||
Range: OFF|GEA1|GEA2|GEA3 | ||
0|OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SECurity:Ciphering:GPRS:ALGorithm GEA3" ! Sets the ciphering GPRS algorithm to GEA3. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This parameter sets which ciphering algorithm will be used for GSM voice or circuit switched data.See GSM Ciphering Algorithm for more information |
|
EGPRS LA | ||
Range: OFF|A51|A53 | ||
Range: OFF|A51|A53 | ||
0|OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:SECurity:Ciphering:GSM:ALGorithm A53" ! Sets the ciphering GSM algorithm to A53. |