This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
Sets/Queries which channel has being maped to the fading capable source. Note: the traffic channel includes Tch in GSM and PDCH in (E)GPRS. See Digital Bus Information for more details. |
|
EGPRS LA | ||
Range: BROadcast|TRAFfic | ||
TRAF | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:DBUS:CHAN BRO" ! Map the Broadcast to the fading capable source. |