Last updated: January 18, 2010
Stops any and all measurements that are active. See Measurement States If the trigger arm is set to single, see Trigger Arm (Single or Continuous) Description the measurements will go to the idle state. If the trigger arm is set to continuous the measurements will re-arm and initiate again. |
||
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"ABORT:ALL" ! Aborts all active measurements in progress. |
Stops the selected measurement if it is active. See Measurement States If the trigger arm is set to single, see Trigger Arm (Single or Continuous) Description the measurements will go to the idle state. If the trigger arm is set to continuous the measurements will re-arm and initiate again. |
||
meas- mnemonic |
GSM TA |
AAUDio | BERRor | DAUDio | DPOWer | FBERror|FSTability | IQTuning | MTAudio | ORFSpectrum | PCALibration | PFERror | PVTime | SMONitor | TXPower |
GPRS TA |
BLERror | DPOWer |FSTability| GBERror | IQTuning | MTAudio | ORFSpectrum | PCALibration | PFERror | PVTime | SMONitor | TXPower |
|
GSM/GPRS LA |
AAUDio | BERRor|BFI | BLERror | DAUDio | DPOWer | FBERror|FSTability | GBERror | GPESquality|IFERror| IQTuning | MTAudio | ORFSpectrum | PCALibration | PFERror | PVTime | SMONitor | TXPower |
|
AAUDio | BERRor | BLERror | DAUDio | DPOWer | EDPower|EMACcuracy | ETXPower | FBERror |FSTability| GBERror | IQTuning | MTAudio | ORFSpectrum | PCALibration | PFERror | PVTime | SBERror |SMONitor | TXPower |
||
AAUDio | BERRor | BFINdication | BFI |BLERror | DAUDio | DPOWer | EDPower|EMACcuracy | ETXPower | FBERror | FFERate|FSTability| GBERror| GPESquality |IFERror| IQTuning | MTAudio | ORFSpectrum | PCALibration | PFERror | PVTime | SBERror |SMONitor | TXPower |
||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.01 and above |
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above |
|
OUTPUT 714;"ABORT:PVTIME" ! Aborts a PvT measurement. |