Last updated: December 3, 2008
Sets/queries the audio generator pulse state. The pulse state must be on when the test set's audio generator is used for audio stimulation during a decoded audio measurement. When the state is on, the audio signal from the test set is pulsed at a 10 Hz rate with a 50% duty cycle. The amplitude and frequency of the pulse is set with afgenerator commands. See AFGenerator . |
||
GPRS TA | ||
Setting | Range: 0 | OFF | 1 | ON | |
*RST setting | 0 | OFF | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"AFGENERATOR:PULSE ON" ! Sets the audio generator pulse to ON. |