Last updated: December 3, 2008
Function | GSM TA |
This command sets/queries the band in which the broadcast channel (BCH) is transmitted. If this parameter is changed to PCS or DCS the Band Indicator changes to match this setting. The Band Indicator is not affected by other settings to the BCH Cell Band. The command to set the Band Indicator is CALL[:CELL]:BINDicator . |
Range: PGSM | DCS | EGSM | GSM450 | GSM480 | GSM750 | GSM850 | PCS | RGSM | TGSM810 |
||
Range: PGSM | DCS | EGSM | GSM450 | GSM480 | GSM750 | GSM850 | PCS | RGSM | TGSM810 |
||
The *RST value of this command depends on the format currently active. For example, if the GSM format is currently active, the *RST value for this command is the value equivalent to that generated by the command containing the :GSM format identifier. |
||
GSM |
See Cell Band Parameter . |
|
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:BAND PGSM" ! Sets the band for the BCH to PGSM. |