Last updated: December 3, 2008
GSM TA |
Sets/queries the value of the BCC (Base Station Colour Code) for the active format which is the selected format. This can only be set when the Cell Activated State parameter is set to Off (see CALL:OPERating:MODE ). The Expected Burst parameter should be set in addition to the BCC parameter when the test set's operating mode will be set to one of the Test Mode Operating Modes .The Expected Burst parameter allows you to configure the test set to expect a certain uplink midamble pattern (TSC0 through TSC7). The command to configure the Expected burst parameter is CALL:BURSt:TYPE[:SELected] . |
|
GSM/GPRS LA | ||
Related Topics | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:BCCode 4" ! Sets the cell's base station color code to 4. |