Last updated: December 3, 2008
GSM TA |
Sets/queries the value of the Band Indicator. If the BCH Cell Band is changed to DCS or PCS, the Band Indicator is updated to match the BCH Cell Band setting. Changes to the TCH or PDTCH traffic bands do not affect the Band Indicator setting. Also, presetting the test set reverts the Band Indicator setting to its default setting. The command to change the BCH Cell Band is CALL[:CELL]:BAND<[:SELected]|:GSM> . |
|
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision A.06.20 adds the behavior to change the Band Indicator to match the BCH Cell Band. |
GSM/GPRS/ EGPRS LA |
Revision D.03 adds the behavior to change the Band Indicator to match the BCH Cell Band. |
|
OUTPUT 714;"CALL:BINDicator PCS" !Sets the band indicator to PCS. |