Last updated: December 3, 2008
This command sets the RACH and page counters' count to zero. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:COUNt:CLEar:RAPage" ! Clears the RACH and page counters. |
GSM TA | ||
GPRS TA | ||
EGPRS TA | ||
This query returns 600 comma-separated trace values for spreadsheet plotting. These values represent the most recent 10 minute trace data collection period. If the graph is frozen (see How Do I Use the Data Throughput Monitor? ), this command will not return values representative of the graph. If you would like to see the graph this command will return values for, resume the graph then query the trace values. |
||
Revision: D.01 and above | ||
OUTPUT 714;"CALL:COUNt:DTMonitor:OTATx:TRACe?" ! Queries OTA Tx trace data values. OUTPUT 714;"CALL:COUNt:DTMonitor:OTARx:TRACe?" ! Queries OTA Rx trace data values. OUTPUT 714;"CALL:COUNt:DTMonitor:IPTX:TRACe?" ! Queries IP Tx trace data values. OUTPUT 714;"CALL:COUNt:DTMonitor:IPRX:TRACe?" ! Queries IP Rx trace data values. |
GSM TA | ||
GPRS TA | ||
EGPRS TA | ||
This query returns 600 comma-separated trace values for the 10-minute trace data collection period captured prior to the most recent. To find out how many 10-minute periods have elapsed, see CALL:COUNt:DTMonitor[:ALL]:TRACe:HISTory:UNUMber? . |
||
Revision: D.01 and above | ||
OUTPUT 714;"CALL:COUNt:DTMonitor:OTATx:TRACe:HISTory?" ! Queries OTA Tx trace data values. OUTPUT 714;"CALL:COUNt:DTMonitor:OTARx:TRACe:HISTory?" ! Queries OTA Rx trace data values. OUTPUT 714;"CALL:COUNt:DTMonitor:IPTX:TRACe:HISTory?" ! Queries IP Tx trace data values. OUTPUT 714;"CALL:COUNt:DTMonitor:IPRX:TRACe:HISTory?" ! Queries IP Rx trace data values. |
This command is not applicable to the GPRS test application. |
||
EGPRS TA | This command is not applicable to the EGPRS Test Application. | |
Queries the data transmitted from and received by the device being tested. Data is returned in the following order: packets transmitted, bytes transmitted, packets received, bytes received. The function connection type must be set to AUTO by CALL:FUNCtion:CONNection:TYPE . If the data type is not AUTO, this query will return 9.91 E+37. |
||
Requirements | Revision: C.01 and above | |
OUTPUT 714;"CALL:COUNt:MS:IP:ALL?" |
This command is not applicable to the GPRS test application. |
||
EGPRS TA | This command is not applicable to the EGPRS Test Application. | |
Queries the data received by the device being tested. Data is returned in the following order: packets received, bytes received. The connection type must be set to AUTO. See CALL:FUNCtion:CONNection:TYPE . If the data type is not AUTO, this query will return 9.91 E+37. |
||
Requirements | Revision: C.01 and above | |
OUTPUT 714;"CALL:COUNt:MS:IP:RX?" |
This command is not applicable to the GPRS test application. |
||
EGPRS TA | This command is not applicable to the EGPRS Test Application. | |
GSM/GPRS LA |
Queries the data transmitted by the device being tested. Data is returned in the following order: packets transmitted, bytes transmitted. The data connection type must be set to AUTO. See CALL:FUNCtion:CONNection:TYPE . If the data type is not AUTO, this query will return 9.91 E+37. |
|
Requirements | Revision: C.01 and above | |
OUTPUT 714;"CALL:COUNt:MS:IP:TX?" |
This command is not applicable to the GPRS test application. |
||
EGPRS TA | This command is not applicable to the EGPRS Test Application. | |
GSM/GPRS LA |
Queries the number of PRACHs received. See PRACH Length for more information. |
|
Requirements | Revision: C.01 and above | |
OUTPUT 714;"CALL:COUNt:PRACh?" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
EGPRS TA | This command is not applicable to the EGPRS Test Application. | |
This command sets/quires the maximum number of TDMA frames the mobile station is allowed to take for a channel assignment. See Max Frames Allowed for Assignment Parameter for more information. |
||
EGPRS LA | ||
RST setting | 28 | |
Requirements | Revision: C.01 and above | |
OUTPUT 714;"CALL:COUNt:TDMA:FRAMes?" |