This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command returns the following results: packets transmitted, packets received, percentage of packets lost, minimum round trip time (in seconds), average round trip time (in seconds), maximum round trip time (in seconds).
This command will return 9.91 E+37 (NAN) if the |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:DATA:PING:ALL?" ENTER 714;Pxmit,Prcvd,Plost,Min_time,Avg_time,Max_time |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command queries the number of packets received from the DUT or from the alternate device if CALL:DATA:PING:SETup:DEVice is set to ALTernate.
This command will return 9.91 E+37 (NAN) if the |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:DATA:PING:PACKETS:RX?" ENTER 714;variable_name ! Queries the number of packets received from the device being tested. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This queries the number of packets transmitted from the test set.
This command will return 9.91 E+37 (NAN) if the |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:DATA:PING:PACKETS:TX?" ENTER 714;variable_name ! Queries the number of packets transmitted from the test set. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command queries the percentage of packets lost during the ping session.
This command will return 9.91 E+37 (NAN) if the |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:DATA:PING:PLOSS?" ENTER 714;variable_name ! Queries the percentage of lost packets. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This sets/queries the alternate internet protocol (IP) address. This address will be used as the address to ping instead of the device under test if the CALL:DATA:PING:SETup:DEVice command is set to ALT. |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:DATA:PING:SETUP:ALTERNATE:IP:ADDRESS `192.168.16.57'" |
This sets/queries the Alternate internet protocol version 6(IPv6) pinging address. This address will be used as the alternate address to ping instead of the device under test if the CALL:DATA:PING:SETup:DEVice command is set to ALT and the CALL:DATA:PING:SETup:PROTocol command is set to IP6. |
|
Range: 0 to 45 characters of an valid IPv6 address, this can be a normal 39- character IPv6 address, a zero compression IPv6 address or a up to 45-character IPv4 address-compatible address (see IPv6 Address Requirements ). Rangs are from |
|
Range: "" (blank field) or 39 characters of IPv6 address with the format: AAAA:BBBB:CCCC:DDDD:EEEE:FFFF:GGGG:HHHH. Each of the A, B, ... H is an hex number ranging from 0 to F. | |
FE80:0000:0000:0000:0000:0000:0000:0001 | |
Requirements | Lab Application Revision: G.00.08 and above. |
OUTPUT 714;"CALL:DATA:PING:SETUP:ALTERNATE:IP:ADDRESS:IP6 '2009::146.208.232.220'" Sets the alternate Ping6 Address to 2009::146.208.232.220. OUTPUT 714;"CALL:DATA:PING:SETUP:ALTERNATE:IP:ADDRESS:IP6 'FE80::1'" Sets the alternate Ping6 Address to FE80::1. |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command set/queries the number of ping IP messages sent for each uninterrupted invocation of the
CALL:DATA:PING:STARt
command. The |
|
EGPRS LA | ||
10 | ||
Requirements | GSM/GPRS/ EGPRS LA |
Revision: C.01 and above |
OUTPUT 714;"CALL:DATA:PING:SETUP:COUNT 20" |
This command sets/queries the number of bytes sent by the test set in each ping packet when the CALL:DATA:PING:SETup:PROTocol command is set to IP4. |
|
Same as setting | |
Requirements | |
64 bytes | |
OUTPUT 714;"CALL:DATA:PING:SETup:PACKet 10" |
This command sets/queries the number of bytes sent by the test set in each ping packet with the CALL:DATA:PING:SETup:PROTocol command set to IP6. |
|
Same as setting | |
Requirements | Lab Application Revision: G.00.08 and above |
64 bytes | |
OUTPUT 714;"CALL:DATA:PING:SETup:PACKet:IP6 10" |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command queries the average round trip time (in seconds) for a series of pings.
This command will return 9.91 E+37 (NAN) if the |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:DATA:PING:TIME:AVERAGE?" ENTER 714;variable_name |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command queries the maximum round trip time (in seconds) for a series of pings.
This command will return 9.91 E+37 (NAN) if the |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:DATA:PING:TIME:MAXIMUM?" ENTER 714;variable_name |
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command queries the minimum round trip time (in seconds).
This command will return 9.91 E+37 (NAN) if the |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:DATA:PING:TIME:MINIMUM?" ENTER 714;variable_name |