Last updated: December 3, 2008
Function | GSM TA |
This command is not applicable to the GSM Test Applications. |
This command is not applicable to the GPRS Test Applications. |
||
This command is not applicable to the EGPRS Test Applications. |
||
This command sets/queries the state of the Dual Transfer Mode feature. See DTM Enable for more information. Note: The Operating Mode must be set to Cell Off before setting this parameter. See CALL:OPERating for more details. |
||
1|ON | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:CELL:DTMode ON" ! Enables Dual Transfer Mode. |
Function | GSM TA |
This command is not applicable to the GSM Test Applications. |
This command is not applicable to the GPRS Test Applications. |
||
This command is not applicable to the EGPRS Test Applications. |
||
This command sets/queries the state of the Enhanced Dual Transfer Mode feature. See Enhanced DTM Enable for more information. Note: The Operating Mode must be set to Cell Off before setting this parameter. See CALL:OPERating for more details. |
||
0|OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:CELL:DTMode:ENHanced ON" ! Enables Enhanced Dual Transfer Mode. |