Function
|
GSM TA
|
This command is not applicable to GSM.
|
GPRS TA
|
This command is not applicable to GPRS TA. |
GSM/GPRS LA
|
This command is not applicable to GSM/GPRS LA. |
EGPRS TA |
This command sets/queries the RLC/MAC header state, see
RLC/MAC Header State
for detailed information.This setting is only applicable when the operating mode is set to "EGPRS Test Mode BCH+PDTCH" or "EGPRS Test Mode BCH+PDTCH+TCH" |
EGPRS LA
|
Setting
|
Range: UPLink | DOWNlink
|
Query
|
Range: UPLink | DOWNlink
|
*RST Setting
|
UPLink
|
Requirements |
EGPRS TA |
Revision: A.10 and above
|
EGPRS LA |
Revision: G.00.00 and above
|
Programming Example
OUTPUT 714;"CALL:EBPTest:EXPected:RLCMac[:HEADer] DOWN"
! set the RLC/MAC header state to downlink.
|