Last updated: December 3, 2008
This command applies to GSM as described in the GPRS description. This command applies the deferred TCHannel parameters to the active TCH. These parameters are:
|
||
This command applies the deferred PDTCH parameters to the active PDTCH. These parameters are:
For more information on the use of deferred parameters see Using Deferred Parameters . The action taken when this command is set depends on the setting of the cell operating mode and the data connection status:
|
||
GSM/GPRS LA |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:HANDover:IMMediate" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command initiates the network initiated handovers and cell reselections in the two cell test system. The type of cell transition performed by the test set upon receipt of this command depends on the current connection status of DUT. If a voice, CSD or DTM session is currently in progress. a "Handover command" message is sent to the DUT requesting it performs a Handover. If the DUT is in Idle mode (but at least GPRS attached) or a GPRS /EGPRS data connection is in progress, a Packet Cell Change Order message is sent to the DUT requesting it perform cell reselection. see Two-Cell Test System for more information. |
|
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:IMMediate" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command quires the Synchronization Status. The parameter is 1 if the slave test set believes it is synchronized to the master test set. See Handover Parameters for more information. |
|
Query | Range: 0|1 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:INFormation:FSYNch:STATus?" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command quires the Mobile Observed Time Difference value reported in the HANDOVER_COMPLETE message. See Handover Parameters for more information. |
|
Query | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:INFormation:OTDifference?" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command sets/quires the packet-switched handover state. When the PS handover state is set to ON, the handover of a DUT in packet transfer state will maintain packet resources during the handover procedure. otherwise, the DUT must abort the packet resources during the handover procedure. see PS Handover Procedure for more information. |
|
Setting | Range: 1|ON|0|OFF | |
Query | Range: 0|1 | |
*RST setting | 0|OFF | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:PSWitched:STATe ON" ! Sets the PS handover state to ON. |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command sets/quires the Sychronization Indication state. When the Sychronization Indication state is set to ON, the Sychronization Indication IE is present in the HANDOVER_COMMAND message. See Synchronized Handovers for more information. |
|
Setting | Range: 1|ON|0|OFF | |
Query | Range: 0|1 | |
*RST setting | 0|OFF | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:SYNChronize:INDication OFF" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command sets/quires the Normal Cell Indication state. When the Normal Cell Indication state is set to ON, the Normal Cell Indication IE is present in the HANDOVER_COMMAND message. See Synchronized Handovers for more information. |
|
Setting | Range: 1|ON|0|OFF | |
Query | Range: 0|1 | |
*RST setting | 0|OFF | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:SYNChronize:NCI OFF" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command sets/quires the Report Observed Time Difference (ROT) state. When the ROT state is set to ON, the Timing Difference IE is present in the HANDOVER_COMMAND message. The Timing Difference value is controlled by the timing advance values in the two test sets of the two-cell test system:
Where: See Synchronized Handovers for more information. |
|
Setting | Range: 1|ON|0|OFF | |
Query | Range: 0|1 | |
*RST setting | 0|OFF | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:SYNChronize:ROT OFF" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command sets/quires the Timing Advance state. When the Timing Advance state is set to ON, the Timing Advance IE is present in the HANDOVER_COMMAND message. See Synchronized Handovers for more information. |
|
Setting | Range: 1|ON|0|OFF | |
Query | Range: 0|1 | |
*RST setting | 0|OFF | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:SYNChronize:TADVance OFF" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command sets/quires the Synchronization Type. See Synchronized Handovers for more information. |
|
Setting | Range: NON | SYNChronized | PRE | PSEudo | |
Query | Range: NON | SYNC | PRE | PSE | |
*RST setting | NON | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:EXTernal:SYNChronize:TYPE NON" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
Commands the slave test set to align its BCH frame structure with the master's. See Frame Synchronization for more information. |
|
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:FSYNchronize" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command configures the Bit Offset used during Frame Synchronization. See Frame Synchronization for more information. |
|
Setting | ||
Query | ||
*RST setting | 0 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:FSYNchronize:OFFSET:BIT 0" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command configures the Frame Number Offset used during Frame Synchronization. See Frame Synchronization for more information. |
|
Setting | ||
Query | ||
*RST setting | 0 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:FSYNchronize:OFFSet:FNUMber 0" |
This command is not applicable to GSM Test Application | ||
This command is not applicable to GPRS Test Application | ||
This command is not applicable to EGPRS Test Application | ||
GSM/GPRS LA |
This command configures the Power Correction Gain. The Power Correction Gain is a value by which the power level that the master is instructed to output is decreased to compensate for gains in the RF path between the master and slave. See Frame Synchronization for more information. |
|
Setting | ||
Query | ||
*RST setting | 0 | |
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:HANDover:FSYNchronize:POWer:CORRection:GAIN 0" |