Last updated: December 3, 2008
GSM TA |
Sets/queries the value of the cell's Location Area Code (LAC). This can only be set when the Cell Operating Mode parameter is set to Off (see CALL:OPERating:MODE ). |
|
GPRS TA | ||
EGPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:LACODE 456" ! Sets the cell's location area code 456. |
GSM TA |
Sets/queries the value of the cell's Location Area Code (LAC) for the active (that is the selected) format. This can only be set when the Cell Operating Mode parameter is set to Off (see CALL:OPERating:MODE ). |
|
GPRS TA | ||
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:LACODE:SELECTED 456" ! Sets the cell's location area code 456. |
GSM TA |
Sets/queries the value of the cell's Location Area Code (LAC) for the GSM format. This can only be set when the Cell Operating Mode parameter is set to Off (see CALL:OPERating:MODE ). |
|
GSM/GPRS LA | ||
GPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:LACODE:GSM 456" ! Sets the cell's location area code 456. |