Last updated: December 3, 2008
Performs a BS Originated call. See Call Processing Event Synchronization . Additional commands can be appended to aid in controller/Mobile Station synchronization. See Call Processing Subsystem Overlapped Command Synchronization Commands for examples. |
||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:ORIGinate:SEQuential" ! Orignates a base station call. ! Appending SEQuential to this command ! causes the command to be performed sequentially. |
This command sets/queries the Call Originate Timeout parameter. This parameter sets the Timer 301 (T301), which controls the time the test set alerts a mobile station when attempting a mobile terminated call. The Call Originate Timeout parameter may be set in any operating mode, but is only used for mobile terminated calls when the operating mode is Active Cell ( Serving Cell GSM, GPRS or EGPRS). See How Do I Change Paging Parameters? for information on how to manually configure this the Call Originate Timeout Parameter. |
||
10 seconds | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:ORIGinate:TIMeout" ! Sets the Call Originate Timeout parameter to 15 seconds. |