Last updated: December 3, 2008
GSM TA |
Sets/queries the value of the Routing Area Code (RAC). This can only be set when the Call Operating Mode parameter is set to Off (see CALL:OPERating:MODE ). |
|
Related Topics | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:RACODE 111" ! Sets the cell's routing area code to 111. |