Sets/queries the RF Generator mode:
Normal: This mode is the normal CW operating mode is in which the test set generates a CW signal. Operating mode = Test Mode and Downlink Function = CW. See CW . See FM Broadcast for more information. GPS: In this mode, the test set generates the required GPS signal at specified frequency point and specified power level. See Single Channel GPS Source for more information |
||
EGPRS TA | ||
Range: NORM | FMBR |GPS | ||
NORMal | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:CONFigure FMBRoadcast" ! Sets RF Generator mode to FM Broadcast. |
Sets/queries the loss of the FM Adapter. This parameter compensates the loss by increasing the signal strength at the RF OUT ONLY port. Operating mode = Test Mode and Downlink Function = CW. See CW . See FM Broadcast for more information. |
||
EGPRS TA |
||
-19.75 dB | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:ADAPter:GAIN -19.75" ! Sets FM Broadcast Adapter Gain to -19.75 dB. |
Sets/queries the FM Broadcast mode Amplitude Offset setting that is applied to the RF OUT ONLY port. Operating mode = Test Mode and Downlink Function = CW. See CW . See FM Broadcast for more information. |
||
EGPRS TA |
||
0 dB | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:CORRection:GAIN 0" ! Sets FM Broadcast Correction Gain to 0 dB. |
Sets/queries whether the FM Broadcast mode Amplitude Offset setting is applied. Operating mode = Test Mode and Downlink Function = CW. See CW . See FM Broadcast for more information. |
||
EGPRS TA |
||
Range: 1 | 0 | ||
OFF | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:CORRection:STATe 0" ! Sets FM Broadcast Correction State to OFF. |
Sets/queries the frequency at which the test set broadcasts the FM signal. Operating mode = Test Mode and Downlink Function = CW. See CW . The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. See FM Broadcast for more information. |
||
EGPRS TA |
||
98.1 MHz | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:FREQuency 100" ! Sets FM Broadcast Frequency to 100 Hz. |
Sets/queries FM Deviation of the internal audio source. The internal audio source is the amount the modulated signal deviates from the carrier frequency. Operating mode = Test Mode and Downlink Function = CW. See CW . The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. See FM Broadcast for more information. |
||
EGPRS TA |
||
22.5 kHz | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:FM:INTernal 22.5 kHz" ! Sets Internal FM Deviation to 22.5 kHz. |
Sets/queries the test set's internal FM frequency. Operating mode = Test Mode and Downlink Function = CW. See CW . The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. See FM Broadcast for more information. |
||
EGPRS TA |
||
1 kHz | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:FM:INTernal:FREQuency 1 kHz" ! Sets the Internal FM Frequency to 1 kHz. |
Sets/queries whether the FM Broadcast mode Internal FM Deviation setting is applied. Operating mode = Test Mode and Downlink Function = CW. See CW . See FM Broadcast for more information. |
||
EGPRS TA |
||
Range: 1 | 0 | ||
1 (ON) | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:FM:INTernal:STATe ON" ! Sets Internal FM Deviation State to ON. |
Sets/queries the power at which the test set broadcasts the FM signal. Operating mode = Test Mode and Downlink Function = CW. See CW . See FM Broadcast for more information.
|
||||
EGPRS TA |
||||
-50 dBm | ||||
Requirements |
GSM/GPRS/ EGPRS TA |
|||
GSM/GPRS/ EGPRS LA |
||||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:POWer -50 dBm ! Sets FM Broadcast Power Amplitude to -50 dBm. |
Sets/queries whether the FM Broadcast Power setting is applied. Operating mode = Test Mode and Downlink Function = CW. See CW . See FM Broadcast for more information. |
||
EGPRS TA |
||
Range: 1 | 0 | ||
1 (ON) | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
||
OUTPUT 714;"CALL:RFGenerator:FMBRoadcast:POWer:STATe ON" ! Sets FM Broadcast Power State to ON. |
Sets/queries the RF Generator Frequency for the active (that is the selected) format. Operating mode = Test Mode and Downlink Function = CW. See CW . The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. |
||
EGPRS TA |
||
The *RST value of this command depends on the format that is currently active. For example, if the GSM format is currently active, the *RST value for this command is the same value as the equivalent command containing the: GSM format identifier. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:RFGenerator:FREQUENCY:SELECTED 896.2MHZ" ! Sets RF Gen frequency. |
Sets/queries the RF Gen Frequency for the GSM format whether or not that format is active. Operating mode = Test Mode and Downlink Function = CW. See CW . The units (Hz|kHz|MHz|GHz) are optional, if no units are specified then units default to Hz. |
||
EGPRS LA |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:CELL:RFGenerator:FREQUENCY:GSM 896.2MHZ" ! Sets RF Gen frequency. |
Sets/queries the filter that is used to filter the GPS baseband signal. A Gaussian or Rectangle filter with 10 MHz bandwidth is supported in this setting. Operating mode = CW. See CW . RF Gen Config = GPS. See Single Channel GPS Source . |
||
EGPRS TA | ||
GAUSsian | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:RFGenerator:GPS:BFILter GAUSsian" ! Sets the type of filter to be GAUSsian |
Queries the frequency of RF source 1. This parameter is fixed at 1575.42MHz and displayed on the MUI. Operating mode = CW. See CW . RF Gen Config = GPS. See Single Channel GPS Source . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:RFGenerator:GPS:FREQuency?" ! Queries the frequency of RF source 1. It will return the value:+1.57542000E+009 |
Queries the frequency of RF source 2. This parameter is fixed at 871MHz. RF source 2 is only available in those TA that use two RF Sources. Operating mode = CW. See CW . RF Gen Config = GPS. See Single Channel GPS Source . |
||
EGPRS TA |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:RFGenerator:GPS:FREQuency2?" ! Queries the frequency of RF source 2. It will return the value:+8.71000000E+008 |
Sets/queries the type of GPS navigation message that is transmitted on GPS frames. Default Navigation (also called TLM): the GPS frames is filled according to the default navigation data (Alternating ones and zeros in word 3 through 10) Raw: the GPS frames is filled with PN sequence. Operating mode = CW. See CW . RF Gen Config = GPS. See Single Channel GPS Source . |
||
EGPRS TA |
||
DEFault | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:RFGenerator:GPS:NMESsage RAW" ! Sets the type of GPS navigation message to be RAW |
Sets/queries the power at which the test set generates the GPS signal. Operating mode = CW. See CW . The actual power range is -125dBm to -70dBm. However, it is affected when there is an amplitude offset. See Single Channel GPS Source for more information.
|
||||
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset . |
||||
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset ) |
||||
-80 dBm | ||||
Requirements |
GSM/GPRS/ EGPRS TA |
|||
GSM/GPRS/ EGPRS LA | ||||
OUTPUT 714;"CALL:RFGenerator:GPS:POWer:AMPLitude -80 dBm ! Sets GPS Power Amplitude to -80dBm. |
Sets/queries whether the GPS power setting is applied. Operating mode = CW. See CW . RF Gen Config = GPS. See Single Channel GPS Source . |
||
Range: 1 | 0 | ||
1 |ON | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:RFGenerator:GPS:POWer:STATe ON" ! Sets GPS Power State to ON. |
Sets/queries the power at which the test set generates the GPS signal. Setting this parameter is also set the GPS State to ON. Operating mode = CW. See CW . The actual power range is -125dBm to -70dBm. However, it is affected when there is an amplitude offset. See Single Channel GPS Source for more information.
|
||||
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset . |
||||
Range: -160dBm to -20dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset . |
||||
-80 dBm | ||||
Requirements |
GSM/GPRS/ EGPRS TA |
|||
GSM/GPRS/ EGPRS LA | ||||
OUTPUT 714;"CALL:RFGenerator:GPS:POWer -80 dBm !Sets GPS Power State to ON and Amplitude to -80dBm. |
Sets/queries the date type that is transmitted on GPS frames. Operating mode = CW. See CW . RF Gen Config = GPS. See Single Channel GPS Source . |
||
PN9 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:RFGenerator:GPS:RAW:PPATtern PN15" ! Sets the date type to be PN15 |
Sets/queries which satellite is generating the GPS signal. Operating mode = CW. See CW . RF Gen Config = GPS. See Single Channel GPS Source |
||
1 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:RFGenerator:GPS:SVID 2 !Sets GPS satellite ID to be 2. |