Last updated: January 18, 2010
GSM TA |
Queries the vocoder calibration type. See Calibration Type . |
|
AOP | AIP | ICOD | ||
*RST Setting | AOPath | |
GSM/GPRS/ EGPRS LA | Revision: G.01 and above | |
OUTPUT 714;"CALL:RTVocoder:CALibration:TYPE AOP" !Set the vocoder calibration type to Audio Out Path. |
GSM TA |
Queries the headroom of the decoded data samples to the full scale of the DAC (Digital to Analog Converter). See "Real-Time Vocoder Headroom Information" . |
|
*RST Setting | 9.91E+37 (NAN) | |
GSM/GPRS/ EGPRS LA | Revision: F.00.27 and above | |
OUTPUT 714;"CALL:RTVocoder:DECoder:HEADroom?" ! Queries decoder headroom. |
GSM TA |
Queries the headroom of the audio samples to the full scale of the ADC (Analog to Digital Converter). See "Real-Time Vocoder Headroom Information" . |
|
*RST Setting | 9.91E+37 (NAN) | |
GSM/GPRS/ EGPRS LA | Revision: F.00.27 and above | |
OUTPUT 714;"CALL:RTVocoder:ENCoder:HEADroom?" ! Queries encoder headroom. |
GSM TA |
Sets/queries the peak voltage of the analog audio signal that is applied at the test set's AUDIO IN connector. The units (V|mV) are optional. If no units are specified, then units default to V. See "Setting Real-Time Vocoder Parameters" . |
|
*RST Setting | 2.0 V | |
GSM/GPRS/ EGPRS LA | Revision: F.00.27 and above | |
OUTPUT 714;"CALL:RTVocoder:INPut:VOLTage 350mV" ! Sets the peak level of Audio In signal to 350 mV. |
GSM TA |
Sets/queries the vocoder operating mode. See Operating Mode . |
|
Range: NORMal | CALibration | ||
Range: NORM | CAL | ||
*RST Setting | NORMal | |
GSM/GPRS/ EGPRS LA | Revision: G.01 and above | |
OUTPUT 714;"CALL:RTVocoder:OPER:MODE NORM" !Sets the vocoder operating mode to Normal. |
GSM TA | Sets the vocoder Audio Out Frequency, see Audio Out Frequency . | |
same as setting | ||
*RST Setting | 1000Hz | |
GSM/GPRS/ EGPRS LA | Revision: G.01 and above | |
OUTPUT 714;"CALL:RTVocoder:OUTPut:FREQuency 1000Hz" !Sets the vocoder Audio Out Frequency to 1000Hz. |
GSM TA |
Sets/queries the maximum audio peak output level that is produced on the test set's AUDIO OUT connector according to the voice data received on the R-Traffic/R-FCH channel. The units (V|mV) are optional. If no units are specified, then units default to V. See "Setting Real-Time Vocoder Parameters" . |
|
*RST Setting | ||
GSM/GPRS/ EGPRS LA | Revision: F.00.27 and above | |
OUTPUT 714;"CALL:RTVocoder:OUTPut:VOLTage 350MV" ! Sets the peak level of AUDIO OUT signal to 350 mV. |
GSM TA |
Sets/queries whether or not the voice activity detection algorithm is implemented in the speech codec. See "Setting Real-Time Vocoder Parameters" . |
|
*RST Setting | 0|OFF | |
GSM/GPRS/ EGPRS LA | Revision: F.00.27 and above | |
OUTPUT 714;"CALL:RTVocoder:VADetection ON" ! Enable the voice activity detection algorithm. |
GSM TA |
Sets/queries the voice activity detection algorithm. See "Setting Real-Time Vocoder Parameters" . |
|
*RST Setting | ||
GSM/GPRS/ EGPRS LA | Revision: F.00.27 and above | |
OUTPUT 714;"CALL:RTVocoder:VADetection:AMRate:ALGorithm OPT2" ! Select Option 2 VAD algorithm for AMR. |