Last updated: December 3, 2008
GSM TA | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This parameter sets/quires the enhanced power control mode. See EPC Mode for more information. |
|
0 | OFF | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SIGNaling:MS:EPControl:MODE OFF" ! Turns the EPC Mode OFF. |
GSM TA | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This parameter sets/quires whether EPC signalling is used continuously or only when a change is required. See EPC Continuous for more information. |
|
0 | OFF | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SIGNaling:MS:EPControl:CONTinuous OFF" ! Turns the EPC Continuous OFF. |
GSM TA | ||
GPRS TA | This command is not applicable to the GPRS Test Application. | |
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This parameter sets/quires the maximum EPC step size that taken to reach the destination power. See EPC Maximum Step Size for more information. |
|
4 | ||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SIGNaling:MS:EPControl:STEP:MAXimum 4" ! Sets the EPC Maximum Step Size to 4. |
GSM TA |
THIS COMMAND IS OBSOLETE. Please use the command CALL:TCHannel:(FACCH|FACChannel):MS:TXLevel instead. Sets/queries the TX Level FACCH Signaling parameter. When TX Level FACCH Signaling is set to on, the base station emulator uses both a FACCH (Fast Associated Control CHannel) channel assignment and an update to the SACCH (Slow Associated Control CHannel) header to signal the mobile to change to a new power level. When TX Level FACCH Signaling is set to off, the base station emulator uses only an update to the SACCH header to signal the mobile to change to a new power level. A FACCH channel assignment message is not sent. This setting is useful if you want to update the SACCH header's TX Level field without performing a channel assignment. The setting of TX Level FACCH Signaling can be changed in either of the test set's two operating modes, Active Cell or Test mode. |
|
GSM/GPRS LA | ||
GPRS TA | ||
1 | ON | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"CALL:SIGNaling:MS:TXLevel:FACCH 0" ! Turns the TX Level Signaling parameter OFF. |