Last updated: December 3, 2008
Function | GSM TA | This command is not applicable to the GSM test applications. |
This command is not applicable to the GPRS test applications. | ||
This command is not applicable to the EGPRS test applications. | ||
This command sets/queries the TMSI (Temporary Mobile Subscriber Identity). TMSI is described in 3GPP TS 23.003 Section 2.4, which states that "The network shall not allocate a TMSI with all 32 bits equal to 1 (this is because the TMSI must be stored in the SIM, and the SIM uses 4 octets with all bits equal to 1 to indicate that no valid TMSI is available)."
This parameter can only be set while the Call Status is Idle and the Data Connection Status is Idle. (Manually setting the
When the
When the The TMSI value used for both test sets in a Two-Cell Test System is the TMSI setting in the test set that initiates the External Device Connection. |
||
Range: 0 to 4294967294 (Note: The value 4294967295 (or 232 - 1) is reserved by the mobile station to indicate that it does not have a valid TMSI stored.) |
||
21430000 (This value is used in the 3GPP TS 51.010 section 27 conformance test.) | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:TMSI 1234567890" ! Sets the TMSI value. |
Function | GSM TA | This command is not applicable to the GSM test applications. |
This command is not applicable to the GPRS test applications. | ||
This command is not applicable to the EGPRS test applications. | ||
This command sets/queries whether the test set assigns a TMSI to the mobile station during the Location Area Update, Routing Area Update, and Combined GPRS/IMSI Attach procedures. If the This parameter can only be set while the Call Status is Idle and the Data Connection Status is Idle.
You must set
The command to set the
The command to set/query the |
||
OFF | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:TMSI:ASSignment ON" ! Turns on the TMSI procedure. |