Last updated: December 3, 2008
Queries the Dynamic Power measurement results. Query returns N integrity indicators and N average TX power levels (where N is the number of bursts measured). To set the number of bursts you want to measure, use SETup:DPOWer:COUNt:NUMBer[:SELected] . Each of the ranges can query up to 100 bursts. Therefore if you have set up to measure 250 bursts you must use range 1, range 2 and range 3 to obtain all your results. |
||
Integrity indicators for each individual burst
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCh:DPOWer?" ! Queries the Dynamic Power measurement results for the first 100 bursts. |
Queries the intermediate count of measurements completed in a multi-measurement. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCH:DPOWER:ICOUNT?" |
Returns N integrity indicators (where N is the number of bursts measured). To set the number of bursts you want to measure, use SETup:DPOWer:COUNt:NUMBer[:SELected] . Each of the ranges can query up to 100 bursts. Therefore if you have set up to measure 160 bursts you must use range 1 and range 2 to obtain all the integrity indicators. |
||
Range: See Integrity Indicator . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCh:DPOWer:INTegrity:RANGe3?" ! Queries the integrity results for bursts 201 through 300. |
Queries the average TX power levels for the Dynamic Power measurement. Returns N average power levels (where N is the number of bursts measured. To set the number of bursts you want to measure, see SETup:DPOWer:COUNt:NUMBer[:SELected] . Each of the ranges can query up to 100 bursts. Therefore if you have set up to measure 400 bursts you must use range 1, range 2, range 3 and range 4 to obtain all your TX power level results. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCh:DPOWer:POWer:RANGe2?" ! Queries the average TX power for bursts 101 through 200. |
Queries the average offset range for the Dynamic Power measurement. |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCh:DPOWer:RANGe:OFFSet?" ! Queries offset value. |