Last updated: September 1, 2009
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries integrity indicator, RMS error vector magnitude (EVM), peak EVM, 95th percentile EVM, frequency error, origin offset suppression, RMS phase error, RMS magnitude error, amplitude droop, IQ imbalance. |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCh:EMACcuracy:ALL?" ! Returns all of the 8PSK Modulation Accuracy results. |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the ETSI specified 8PSK multislot modulation accuracy results; integrity indicator, RMS error vector magnitude, peak error vector magnitude, 95th percentile, frequency error, and origin offset suppression. |
||
|
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"FETCH:PFERROR:ALL:ETSI?" ! Returns the ETSI-specified 8PSK modulation accuracy results. |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the EGPRS Modulation Accuracy EVM measurement and returns 142 points representing the EVM results (in %) of the trace data. If the graph state is OFF, this query returns NAN. See SETup:EMACcuracy:GRAPh:STATe . When multi-measurements are turned on, this is the trace data for the last burst measured |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the EGPRS Modulation Accuracy Sample EVM Histogram measurement and returns 201 points representing a histogram of the EVM results for the measured burst or bursts. The last point returned is the number of samples whose EVM value exceeded the maximum value allowed by the histogram at its current resolution setting. (See SETup:EMACcuracy:HISTogram:MAXimum:EVM for more information.) If the graph state is OFF, this query returns NAN. See SETup:EMACcuracy:GRAPh:STATe . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the intermediate count of 8PSK modulation accuracy multi-measurements completed. This number will increase to the value returned by SETup:EMACcuracy:COUNt:NUMBer . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the maximum IQ amplitude imbalance result from a multi-measurement. The IQ Imbalance State must be turned on for this query to return a result other than NAN. See SETup:EMACcuracy:IQIMbalance[:CALCulate]:STATe . |
||
Range: -100 dB to 0 dB and 9.91 E+37 (NAN) Resolution: 0.01 dB |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the minimum IQ amplitude imbalance result from a multi-measurement. The IQ Imbalance State must be turned on for this query to return a result other than NAN. See SETup:EMACcuracy:IQIMbalance[:CALCulate]:STATe . |
||
Range: -100 dB to 0 dB and 9.91 E+37 (NAN) Resolution: 0.01 dB |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the average IQ imbalance result from a multi-measurement. The IQ Imbalance State must be turned on for this query to return a result other than NAN. See SETup:EMACcuracy:IQIMbalance[:CALCulate]:STATe . |
||
Range: -100 dB to 0 dB and 9.91 E+37 (NAN) Resolution: 0.01 dB |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the standard deviation result from an IQ amplitude imbalance multi-measurement.The IQ Imbalance State must be turned on for this query to return a result other than NAN. See SETup:EMACcuracy:IQIMbalance[:CALCulate]:STATe . |
||
Range: -20 dB to +20 dB and 9.91 E+37 (NAN) Resolution: 0.01 dB |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA | This command is not applicable to GSM. | |
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
Queries the integrity indicator for the 8PSK multislot modulation accuracy measurement. Zero indicates a normal result. See Integrity Indicator for descriptions of non-zero integrity indicators. |
||
Range: See Integrity Indicator . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |