Last updated: November 25, 2010
The following commands are only applicable to lab applications or the feature-licensed test applications.
GSM TA |
This command sets/queries all the DTS parameters for a specified range of DSSs. The command has a comma separated list of parameters in the following order: <The first DSS>, <The last DSS>, <Frequency>, <Repeat Count>, <Frame Power Level Allocation>, <Burst Type 1>, <Burst Type 2>, <Burst Type 3>, <Burst Type 4>, <Burst Type 5>, <Burst Type 6>. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Same as setting. | ||
939MHz, 1, MIXed, DUMMY, DUMMY, DUMMY, DUMMY, DUMMY, DUMMY | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:ALL 1,2,9e+8,2,PL1,FCB,FSB,DUMMY,DUMMY,DUMMY,DUMMY" ! Sets the frequency, repeat count, frame power level allocation and burst type for both DSS 1 and 2. OUTPUT 714;"GFDTune:DOWNlink:SSTep:ALL 1? ! Queries all the DTS parameters for DSS 1. |
GSM TA |
The command has no query form. This command sets ARFCN for a specified range of DSSs in the following order: <Band Parameter>, <ARFCN>. The <Band Parameter> is optional and specifies whether ARFCNs common to both the DCS and PCS bands should be treated as DCS or PCS, DCS or PCS has no meaning for ARFCNs corresponding to other bands. If the band parameter is not specified, DCS is assumed. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Setting |
|
|
*RST setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:ARFCn 1,3,PCS,512,PCS,513,PCS,514" ! Sets the ARFCN of DSS 1-3 to 512, 513 and 514 respectively in the PCS band. |
GSM TA |
This command sets/queries the Burst Type (per timeslot) of the timeslot 0 to 5 for a specified range of DSSs. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Range: OFF|FCB|FSB|DSB|DUMMY|PRBS|EPSK_PRBS | ||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:BURSt:TYPE:TSLot0 1,2,FCB,FSB" ! Sets the burst type of timeslot 0 for DSS 1-2 to FCB and FSB respectively. |
GSM TA |
This command sets/queries the DTS Frequency for a specified range of DSSs. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Range: 400 to 630 MHz (Band 1), 630 to 1000 MHz (Band 2), 1550 to 2400 MHz (Band 3) |
||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:FREQuency 1,4,850,900,950,1000,1000" ! Sets the frequency for DSS 1-4 to 850, 900, 950, 1000, and 1000MHz respectively. |
GSM TA |
This command sets/queries the Frame Power Level Allocation for a specified range of DSSs. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Same as setting. | ||
MIXed | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:PLEVel:FRAMe 1,10,MIXed" ! Sets the frame power level allocation for DSS 1-10 to MIXed. |
GSM TA |
This command sets/queries the Repeat Count parameter for a specified range of DSSs. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Same as setting. | ||
1 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:REPeat 1,1,10" ! Sets the repeat count to 10 for DSS 1. |
GSM TA |
This command sets/queries the Trigger Frame parameter for a specified range of DSSs. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:TRIGger:FRAMe 1,10,1" ! The trigger event occurs at the first frame in DSS 1-10. |
GSM TA |
This command sets/queries the Trigger State parameter for a specified range of DSSs. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
0|1. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:TRIGger:STATe 1,4,ON" ! Enables the trigger event for DSS 1-4. |
GSM TA |
This command sets/queries the Trigger Timeslot parameter for a specified range of DSSs. See Note1 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:SSTep:TRIGger:TSLot 1,4,0" ! The trigger event occurs at timeslot 0 for DSS 1-4. |
GSM TA |
The command has no query form. This command sets ARFCN for all the DSSs in a DTS in the following order: <Band Parameter>, <ARFCN>. The number of element pairs in the command is given by the DTS Step Count . For example, if the DTS Step Count is 4, then the command should follow with four Band and ARFCN pairs. Note that the <Band Parameter> is optional and specifies whether ARFCNs common to both the DCS and PCS bands should be treated as DCS or PCS, DCS or PCS has no meaning for ARFCNs corresponding to other bands. If this parameter is not specified, DCS is assumed. See Note2 for more information on how to use this command. See DTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Setting |
|
|
*RST setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 5" !Sets the DTS Step Count to 5. OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:ARFCn 975,8,66,124" ! Sets the ARFCN for the five DSSs to 975, 8, 66, 124 and 124 respectively. ! (The ARFCN of Step 5 is equal to Step 4 as there are only four parameters in the command.) |
GSM TA |
This command sets/queries the content in the field of reduced frame number (RFN) in a dynamic synchronization burst (DSB). See DSB RFN Mode for more information. |
|
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.13 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:BURSt:DSBurst:RFNumber SRC" ! Sets the DSB RFN mode to SRC. |
GSM TA |
This command sets/queries the Burst Type (per timeslot) parameter for timeslot <n>, where <n> can be any integer from 0 to 5, for all the DSSs in a DTS. See Note2 for more information on how to use this command. |
|
GSM/GPRS LA | ||
Range: OFF|FCB|FSB|DSB|DUMMY|PRBS | ||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 5" !Sets the DTS Step Count to 5. OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:BURSt:TYPE:TSLot0 FCB,DUMMY" ! Sets the burst type of timeslot 0 to FCB for the 1st DSS and DUMMY to DSS 2-5. ! (The burst type of DSS 3-5 are all equal to DSS 2 as there are only two parameters in the command.) |
GSM TA | This command sets/queries the DTS Continuous parameter. | |
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:CONTinuous 0" ! Sets the DTS to be generated once. |
GSM TA |
This command sets/queries the DTS Frequency parameter for all the DSSs in a DTS. See Note2 for more information on how to use this command. |
|
GSM/GPRS LA | ||
Range: 400 to 630 MHz (Band 1), 630 to 1000 MHz (Band 2), 1550 to 2400 MHz (Band 3) |
||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 5" !Sets the DTS Step Count to 5. OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:FREQuency 8.5e+8, 9e+8, 9.5e+8, 1e+9" ! Sets the frequency for the five DSSs to 850, 900, 950, 1000 and 1000 MHz, respectively. ! (The frequency of Step 5 is equal to Step 4 as there are only four parameters in the command.) |
GSM TA |
This command sets/queries the Frame Power Level Allocation parameter for all the DSSs in a DTS. See Note2 for more information on how to use this command. |
|
GSM/GPRS LA | ||
Same as setting. | ||
MIXed | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 5" !Sets the DTS Step Count to 5. OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:PLEVel:FRAMe PL1,MIXed" ! The power level of all the timeslots in DSS 1 must be PL1. ! The power level of all the timeslots in DSS 2-5 can be assigned power levels PL1 through PL4. |
GSM TA |
This command sets/queries the Power Levels per Timeslot parameter for timeslot <n>, where <n> can be any integer from 0 to 5. |
|
GSM/GPRS LA | ||
Same as setting. | ||
PL1 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:PLEVel:TSLot1 PL2" ! Sets the power levels of timeslot 1 for all the DSSs to PL2. |
GSM TA |
This command set/queries the DTS Power Level . |
|
GSM/GPRS LA | ||
Same as setting. | ||
PL1 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:PLEVel1 -50" ! Sets the power level 1 (PL1) to -50 dBm. |
GSM TA |
This command sets/queries the Repeat Count parameter for all the DSSs in a DTS. See Note2 for more information on how to use this command. |
|
GSM/GPRS LA | ||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 5" !Sets the DTS Step Count to 5. OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:REPeat 10,1,1,2" ! Sets the repeat count for the DSS 1-5 to 10, 1, 1, 2 and 2 respectively. ! (The repeat count of Step 5 is equal to Step 4 as there are only four parameters in the command.) |
GSM TA | This command sets/queries the DTS Step Count parameter. | |
GSM/GPRS LA | ||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 10" ! Sets the number of DSSs in the DTS to 10. |
GSM TA | This command starts the Downlink Test Sequence. See DTS Start for more information. | |
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:STARt" ! Starts the transmission of DTS. |
GSM TA | This command stops the Downlink Test Sequence. See DTS Stop for more information. | |
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:STOP" ! Stops the transmission of DTS. |
GSM TA |
This command sets/queries the Trigger Frame parameter at which the external trigger event occurs for all the DSSs in a DTS. See Note2 for more information on how to use this command. |
|
GSM/GPRS LA | ||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 5" !Sets the DTS Step Count to 5. OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:TRIGger:FRAMe 1,10,1" ! The external trigger event of DSS 1-5 occurs at 1st, 10th , 1st, 1st, and 1st frame respectively. |
GSM TA |
This command sets/queries the Trigger State parameter that controls the external trigger output for all the DSSs in a DTS. See Note2 for more information on how to use this command. |
|
GSM/GPRS LA | ||
0|1 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 5" !Sets the DTS Step Count to 5. OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:TRIGger:STATe 1,1,1,1,0" ! Enables the external trigger output for DSS 1-4 and diables the external trigger output for DSS 5. |
GSM TA |
This command sets/queries the Trigger Timeslot on which the external trigger event occurs for all the DSSs in a DTS. See Note2 for more information on how to use this command. |
|
GSM/GPRS LA | ||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:SSTep 5" !Sets the DTS Step Count to 5. OUTPUT 714;"GFDTune:DOWNlink:TSEQuence:TRIGger:TSLot 3,3, 2" ! The external trigger event occurs to timeslot 3 on DSS1, timeslot 3 on DSS2 and timeslot 2 on DSS 3-5. |
This command sets/queries the DTS parameters for one or several DSSs. In the setting form, the first two parameters in the command indicate the first and last sequence step to which the following parameters apply. The subsequent parameters are specified as an array of values, where each element of the array correspond to a DSS. The test set compensates by using the value of the last element in the array when there are too few elements and by ignoring settings if there are too many elements in the array. In the querying form, the first parameter indicates the result of which sequence step is returned and the second parameter is omitted. You can only query the DTS parameters for one DSS at a time.
This command sets/queries the DTS parameters on a per DTS basis. The parameters in the command are specified as an array of values, where each element of the array corresponds to a DSS. The number of elements that should be specified in the array is given by the DTS Step Count . If these numbers contradict (that is, the DTS Step Count does not equal the number of array elements specified for the array), the test set compensates by using the value of the last element in the array when there are too few elements and by ignoring settings if there are too many elements in the array.