Last updated: December 3, 2008
The following commands are only applicable to the lab applications or the feature-licensed test applications.
GSM TA |
The command has no query form. This command sets ARFCN for a specified range of USSs in the following order: <Band Parameter>, <ARFCN>. The <Band Parameter> is optional and specifies whether ARFCNs common to both the DCS and PCS bands should be treated as DCS or PCS, DCS or PCS has no meaning for ARFCNs corresponding to other bands. If the band parameter is not specified, DCS is assumed. See Note1 for more information on how to use this command. See UTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Setting |
|
|
*RST setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:UPLink:SSTep:ARFCn 1,3,PCS,512" ! Sets the ARFCN of USS 1-3 to 512 in the PCS band. |
GSM TA |
This command sets/queries the frequency for a specified range of USSs. See Note1 for more information on how to use this command. See UTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Range: 292.2 to 645.5 MHz (Band 1), 645.5 to 1395.5 MHz (Band 2), and 1395.5 to 2700 MHz (Band 3) |
||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:UPLink:SSTep:FREQuency 1,1,9e+8," ! Sets the frequency of USS 1 to 900 MHz. |
GSM TA |
The command has no query form. This command sets ARFCN for all the USSs in a UTS in the following order: <Band Parameter>, <ARFCN>. The number of element pairs in the command is given by the UTS Step Count . For example, if the UTS Step Count is 4, then the command should follow with four Band and ARFCN pairs. Note that the <Band Parameter> is optional and specifies whether ARFCNs common to both the DCS and PCS bands should be treated as DCS or PCS, DCS or PCS has no meaning for ARFCNs corresponding to other bands. If this parameter is not specified, DCS is assumed. See Note2 for more information on how to use this command. See UTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Setting |
|
|
*RST setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:UPLink:TSEQuence:SSTep 5" !Sets the UTS Step Count to 5 OUTPUT 714;"GFDTune:UPLink:TSEQuence:ARFCn 975, 8, 66 ,124" ! Sets the ARFCN for USS 1-5 to 975, 8, 66, 124 and 124 respectively. ! (The ARFCN of USS 5 is equal to USS 4 as there are only four parameters in the command.) |
GSM TA |
This command sets/queries the number of uplink bursts present in the TDMA frame for all the USSs in a UTS. See Note2 for more information on how to use this command. See UTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Same as setting. | ||
1 | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:UPLink:TSEQuence:BURSt:COUNt 4" ! Sets the number of uplink bursts present to 4 |
GSM TA |
This command sets/queries the transmission state of Burst N for all the USSs in a UTS. See UTS Burst State . Note the burst transmission state of all the USSs are the same so the command only have one parameter. See UTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Range: 1|ON|0|OFF |
||
Range: 1|0 | ||
1|ON | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.09 and above, with the required feature license. |
OUTPUT 714;"GFDTune:UPLink:TSEQuence:SSTep 5" !Sets the UTS Step Count to 5 OUTPUT 714;"GFDTune:UPLink:TSEQuence:BURSt2:STATe ON" ! Sets the transmission state of Burst 2 for USS 1-5 to ON. |
GSM TA |
This command sets/queries the frequency of all the USSs in a UTS. See Note2 for more information on how to use this command. See UTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Range: 292.2-645.5 MHz (Band 1), 645.5 to 1395.5 MHz (Band 2), and 1395.5 to 2700 MHz (Band 3) |
||
Same as setting. | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:UPLink:TSEQuence:SSTep 5" !Sets the UTS Step Count to 5 OUTPUT 714;"GFDTune:UPLink:TSEQuence:FREQuency 8.5e+8, 9e+8, 9.5e+8, 1e+9" ! Sets the frequency for USS 1-5 to 850,900, 950, 1000 and 1000MHz respectively ! (The frequency of USS 5 is the same as USS 4 as there are only four parameters in the command.) |
GSM TA |
This command sets/queries the UTS Step Count parameter. See UTS Parameters for additional information. |
|
GSM/GPRS LA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.08 and above, with the required feature license. |
OUTPUT 714;"GFDTune:UPLink:TSEQuence:SSTep 10" ! Sets the number of Uplink Sequence Steps to 10. |
This command sets/queries the UTS parameters for one or several USSs. In the setting form, the first two parameters in the command indicate the first and last sequence step to which the following parameters apply. The subsequent parameters are specified as an array of values, where each element of the array correspond to a USS. The test set compensates by using the value of the last element in the array when there are too few elements and by ignoring settings if there are too many elements in the array. In the querying form, the first parameter indicates the result of which sequence step is returned and the second parameter is omitted. You can only query the UTS parameters for one USS at a time.
This command sets/queries the UTS parameters on a per UTS basis. The parameters in the command are specified as an array of values, where each element of the array corresponds to a USS. The number of elements that should be specified in the array is given by the UTS Step Count . If these numbers contradict (that is, the UTS Step Count does not equal the number of array elements specified for the array), the test set compensates by using the value of the last element in the array when there are too few elements and by ignoring settings if there are too many elements in the array.