Last updated: January 18, 2010
GSM TA |
Starts measurements with the test set. The INITiate command is associated with the SETup command, and the FETCh? command, see SETup Subsystem and FETCh? Subsystem . One or more measurements may be initiated on the same program line. See Concurrent Measurements . This command is also used to activate a measurement. See INITiate Programming Examples (how INIT commands are used) . |
|
GPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"INITIATE:TXPOWER:ON" !Initiates a TX Power measurement. OUTPUT 714;"INITIATE:TXPOWER;PFERROR:ON" ! Initiates TX Power and phase and frequency error measurements. OUTPUT 714;"INITIATE:PVTIME;ORFSPECTRUM;FBERROR:ON" ! Initiates power versus time output RF spectrum, and fast bit error rate measurements. |
GSM TA |
Deactivates the selected measurement. See Measurement States . Only one measurement can be deactivated at a time. To stop one or more measurements and leave them in the active state, see ABORt . |
|
GPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"INITIATE:TXPOWER:OFF" ! Deactivates TX power measurement. |
GSM TA |
Queries the number of measurements that have been initiated (that are active). See Measurement States . |
|
GPRS TA | ||
Note: Some measurements are mutually exclusive, and so cannot be run at the same time as others, and some measurement close all other measurements. See Concurrent Measurements . |
||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
GSM TA |
Queries (one at a time) which measurements if any are available or have timed out. See Measurement Event Synchronization for details on how to use this command. See Measurement States to understand the test set's measurement states. See INITiate:DONE:FLAG:<measurement mnemonic> for include or exclude commands. Note that WAIT is returned when no measurements are done. NONE is returned when all measurements are done. |
|
GPRS TA | ||
GSM TA |
NONE|AAUD|BERR|DAUD|DPOW|FBER|FST|IQT|MTA|ORFS|PCAL |PFER|PVT| SMON| TXP|WAIT |
|
GPRS TA |
NONE|BLER|DPOW|FST|GBER|IQT|ORFS|PCAL |PFER|PVT| SMON| TXP|WAIT |
|
NONE|BLER|DPOW|EDP|EMAC|ETXP|FST|GBER|IQT|ORFS|PCAL| PFER|PVT| SBER|SMON| TXP|WAIT |
||
NONE|AAUD|BERR|BFI|BLER|DAUD|DPOW|FBER|FFER|FST|GBER|GPES| IQT|MTA|ORFS|PCAL| PFER|PVT|SFER|SMON| TXP|WAIT|IFER |
||
NONE|AAUD|BERR|BFI|BLER|DAUD|DPOW|EDP|EMAC|ETXP|FBER|FFER|FST|GBER|GPES|IQT|MTA|ORFS|PCAL| PFER|PVT|SBER|SFER| SMON| TXP|WAIT|IFER |
||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.01 and above |
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above |
GSM TA |
Clears the done flag from all measurements. See INITiate:DONE? . |
|
GPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"INITIATE:DONE:CLEAR" ! Clears done flag. |
GSM TA |
Specifies that all measurements are considered, (included or excluded) when the DONE? query is sent. If a measurements trigger arm, see Trigger Arm (Single or Continuous) Description , has been left in continuous mode, the done flag for that measurement will toggle between DONE and WAIT, see INITiate:DONE? . The INITiate:DONE? query will probably not be able to catch the measurement at the instant it is done, therefore the measurement will never appear to be done. If a measurement trigger arm must be left in continuous mode the user should (exclude) it, using this command, from the INITiate:DONE? query results. Once the INITiate:DONE:FLAG has been set to EXCLude for a measurement, you must send the INCLude command for that measurement in order to query that measurement with, the INITiate:DONE? query. The test set will reset an (excluded measurement) to be an (included measurement) at power on or with any form of preset, see Preset Descriptions . |
|
GPRS TA | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"INITIATE:DONE:FLAG:ALL EXCLUDE" ! Excludes all measurements from contributing the INITIATE:DONE? query, ! see "INITiate:DONE?" on page 6. |
GSM TA |
Specifies which measurements are considered, (included or excluded) when the DONE? query is sent. If a measurements trigger arm, see Trigger Arm (Single or Continuous) Description , has been left in continuous mode, the done flag for that measurement will toggle between DONE and WAIT, see INITiate:DONE? . The INITiate:DONE? query will not be able to catch the measurement at the instant it is done, therefore the measurement will never appear to be done. If a measurement trigger arm must be left in continuous mode the user should (exclude) it, using this command, from the INITiate:DONE? query results. Once the INITiate:DONE:FLAG has been set to EXCLude for a measurement, the user must send the INCLude command for that measurement in order to query that measurement with, the INITiate:DONE? query. The test set will reset any (excluded measurement) to be an (included measurement) at power on or with any form of preset, see Preset Descriptions . |
|
GPRS TA | ||
|
||
|
||
Related Topics | ||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.01 and above |
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above |
|
OUTPUT 714;"INITIATE:DONE:FLAG:PFERROR EXCLUDE" ! Excludes PFERROR measurements from contributing to the INITIATE:DONE? query. |
Queries the names of the measurements (none, one, or more than one) that are ON in a comma separated list of measurement mnemonics. See INITiate:<measurement mnemonic>[:ON] . |
||
EGPRS TA | ||
Range: AAUD|BERR|DAUD|DPOW|FBER|FFER|IQT|MTA|NONE|ORFS| PCAL |PFER|PVT|SMON|TXP |
||
Range: |
||
Range: AAUD|BERR|BFI|BLER|DAUD|DPOW|FBER|FFER|GBER|GPES|IQT|MTA| NONE| ORFS|PCAL|PFER|PVT|SMON|TXP |
||
Range: AAUD|BERR|BFI|BLER|DAUD|DPOW|EDP|EMAC|ETXP|FBER|FFER|GBER|GPES| IQT| MTA|NONE|ORFS|PCAL|PFER|PVT|SBER|SMON|TXP |
||
Requirements |
GSM/GPRS/ EGPRS TA |
Revision: A.01 and above |
GSM/GPRS/ EGPRS LA |
Revision: C.01 and above |