READ

READ

Last updated: January 18, 2010

GPIB Command Conventions

READ:AAUDio[:ALL]?

Function

GSM TA


Queries (initiates and fetches) one analog audio measurement as a sequential operation.

Returns an integrity indicator (see Integrity Indicator ), average analog audio level, average SINAD, average distortion and the average audio frequency. Values are returned in a comma-separated list.

Returns Integrity Indicator, see Integrity Indicator and analog audio (average). The FETCh command should be used to obtain other measurement results. See FETCh:AAUDio .

GSM/GPRS LA

EGPRS LA

GPRS TA

This command is not applicable to GPRS.

EGPRS TA

This command is not applicable to EGPRS.

Query

Integrity indicator

Analog audio (average)

  • Range: 0 to 20 volts
  • Resolution: 0.1mv

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:BERRor[:ALL]?

Function

GSM TA

Queries (initiates and fetches) one RX bit error measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio and Bit Error Count, for the bit type set using SETup:BERRor[:TYPE] . (A similar query, READ:BERRor:FULL? , returns the same results but for all residual, or all non-residual bit types simultaneously.) The FETCh command should be used to obtain other measurement results. See FETCh:BERRor .

GSM/GPRS LA

EGPRS LA

GPRS TA

This command is not applicable to GPRS.

EGPRS TA

This command is not applicable to EGPRS.

Query

Integrity indicator

Bits tested

  • Range: 0 to (<RX bits to test +131) and 9.91E+37 (NAN)
  • Resolution: 1

Bit error ratio

  • Range: 0 to 100 and 9.91E+37 (NAN)
  • Resolution: 1

Bit error count

  • Range: 0 to (<RX bits to test +131) and 9.91E+37 (NAN)
  • Resolution: 1

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:BERRor:FULL?

Function

GSM TA

Queries (initiates and fetches) one RX bit error measurement as a sequential operation. Either all of the residual or non-residual results are returned, depending on the type of bit error measurement set using SETup:BERRor[:TYPE] .

Returns Integrity Indicator (see Integrity Indicator ), Bits Tested, Bit Error Ratio and Bit Error Count for Type Ia, Type Ib and Type II.

(A similar query, READ:BERRor[:ALL]? , returns the same results but only for the bit type previously set using SETup:BERRor[:TYPE] .)

The FETCh command should be used to obtain other measurement results. See FETCh:BERRor .

GSM/GPRS LA

EGPRS LA

GPRS TA

This command is not applicable to GPRS.

EGPRS TA

This command is not applicable to EGPRS.

Query

Integrity indicator

Type Ia Bits tested

  • Range: 0 to 999000 and 9.91E+37 (NAN)
  • Resolution: 1

Type Ia Bit error ratio

  • Range: 0 to 100 and 9.91E+37 (NAN)
  • Resolution: 0.01

Type Ia Bit error count

  • Range: 0 to 999000 and 9.91E+37 (NAN)
  • Resolution: 1

Type Ib Bits tested

  • Range: 0 to 2637369 and 9.91E+37 (NAN)
  • Resolution: 1

Type Ib Bit error ratio

  • Range: 0 to 100 and 9.91E+37 (NAN)
  • Resolution: 0.01

Type Ib Bit error count

  • Range: 0 to 2637369 and 9.91E+37 (NAN)
  • Resolution: 1

Type II Bits tested

  • Range: 0 to 15584400 and 9.91E+37 (NAN)
  • Resolution: 1

Type II Bit error ratio

  • Range: 0 to 100 and 9.91E+37 (NAN)
  • Resolution: 0.01

Type II Bit error count

  • Range: 0 to 1558440 and 9.91E+37 (NAN)
  • Resolution: 1

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:BLERror[:ALL]?

Function

GSM TA

This command is not applicable to GSM.

GPRS TA

Queries (initiates and fetches) one block error measurement as a sequential operation.

Returns Integrity Indicator (see Integrity Indicator ), Blocks Tested, Block Error Ratio, and Block Error Count. The FETCh command should be used to obtain other measurement results. See FETCh:BLERror .

EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Integrity indicator

Blocks tested

  • Range: 0 to 99127 and 9.91E+37 (NAN)
  • Resolution: 1

Block error ratio

  • Range: 0 to 100 and 9.91E+37 (NAN)
  • Resolution: 1

Block error count

  • Range: 0 to 99127 and 9.91E+37 (NAN)
  • Resolution: 1
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:BLERror:BURSt[:ALL]?

Function

GSM TA

This command is not applicable to GSM.

GPRS TA

Queries the block error measurement results for all the bursts. The total integrity indicator and the block error ratio for burst 1 to 8 are returned. Note, the block error ratio for burst 6, 7 and 8 are always NAN. .

This query can only be used when the BLER measurement method is Polling. See Block Error Measurement for more information about the BLER measurement methods.

EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Integrity indicator:

Block error ratio:

  • Range: 0 to 100 and 9.91 E+37 (NAN)
  • Resolution: 0.01
Requirements GSM/GPRS/
EGPRS TA

Revision: A.09 and above

GSM/GPRS/ EGPRS LA

Revision F.01 and above

Programming Example
OUTPUT 714;"READ:BLER:BURS:ALL?"

READ:BLERror:(PDTC2|PDTCH2|PDTChannel2):BURSt[:ALL]?

Function

GSM TA

This command is not applicable to GSM TA.

GPRS TA

This command is not applicable to GPRS TA.

GSM/GPRS LA

This command is not applicable to GSM/GPRS LA.
EGPRS TA

Queries the block error measurement results for all the bursts on Carrier 2. The total integrity indicator and the block error ratio for burst 1 to 8 are returned.

This query can only be used when the BLER measurement method is Polling. See Block Error Measurement for more information about the BLER measurement methods.

EGPRS LA

Query

Integrity indicator:

Block error ratio:

  • Range: 0 to 100 and 9.91 E+37 (NAN)
  • Resolution: 0.01
Requirements GSM/GPRS/ EGPRS LA

Revision H.00.xx and above

Programming Example
OUTPUT 714;"READ:BLER:PDTC2 BURS:ALL?"

READ:BFINdication|BFI[:ALL]?

Function

GSM/GPRS LA

Queries (initiates and fetches) one bad frame indication measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , Number of Samples Counted, Number of Undetected Bad Frames, Number of SIDs Reported as Bad Frames, and the Number of SIDs Sent. The FETCh command should be used to obtain other measurement results. See FETCh:<BFINdication|BFI> .

EGPRS LA

GSM TA This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to GPRS.

EGPRS TA

This command is not applicable to EGPRS.

Query

Integrity indicator

Samples

  • Range: 0 to 999999 and 9.91E+37 (NAN)
  • Resolution: 1

Undetected Bad Frames

  • Range: 0 to 999999 and 9.91E+37 (NAN)
  • Resolution: 1

SIDs marked as BFI

  • Range: 0 to 999999 and 9.91E+37 (NAN)
  • Resolution: 1

SIDs sent

  • Range: 0 to 999999 and 9.91E+37 (NAN)
  • Resolution: 1
Requirements GSM/GPRS/ EGPRS LA

Revision: C.03 and above

READ:DAUDio[:ALL]?

Function

GSM TA

Queries (initiates and fetches) one decoded audio (uplink speech level) measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator and decoded audio (average). The FETCh command should be used to obtain other measurement results. See FETCh:DAUDio .

GSM/GPRS LA

EGPRS LA

GPRS TA

This command is not applicable to GPRS.

EGPRS TA

This command is not applicable to EGPRS.

Query

Integrity indicator

Decoded audio (average)

  • Range: 0 to 100% FS (full scale)
  • Resolution: 0.01% FS

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:DPOWer[:ALL]?

Function

GSM TA Queries the Dynamic Power measurement results. Query returns N integrity indicators and N average TX power levels (where N is the number of bursts measured). To set the number of bursts you want to measure, use SETup:DPOWer:COUNt:NUMBer[:SELected] . The maximum number of results that can be returned is 99. Measurement result 100 and above must be retrieved using the FETCh command.

GSM/GPRS LA

GPRS TA

EGPRS TA

EGPRS LA

Query

Integrity indicators for each individual burst

Average TX power levels for each individual burst

  • Range: -100 to +100 dBm and 9.91 E+37 (NAN)
  • Resolution: 0.01 dBm

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:EDPower[:ALL][:RANGe1|RANGe2|RANGe3|RANGe4|RANGe5|RANGe6|RANGe7|RANGe8|RANGe9|RANGe10]?

Function

GSM TA Queries the EDGE Dynamic Power measurement results. Query returns N integrity indicators and N average TX power levels (where N is the number of measurement results present in the specified range). To set the number of bursts you want to measure, use SETup:EDPower:COUNt:NUMBer .

GSM/GPRS LA

GPRS TA

EGPRS TA

EGPRS LA

Query

Integrity indicators for each individual burst

Average TX power levels for each individual burst

  • Range: -100 to +100 dBm and 9.91 E+37 (NAN)
  • Resolution: 0.01 dB

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.04 and above

Revision A.05 makes the EDP Measurement available in all TAs.

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

Revision D.02 makes the EDP Measurement available in all LAs.

READ:EMACcuracy[:ALL]?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

GSM/GPRS LA

This command is not applicable to the GSM/GPRS LA.

EGPRS TA

Queries (initiates and fetches) the 8PSK multislot modulation accuracy measurement results as a sequential operation.

Queries integrity indicator, RMS error vector magnitude (EVM), peak EVM, 95th percentile EVM, frequency error, origin offset suppression, RMS phase error, peak phase error, RMS magnitude error, peak magnitude error, amplitude droop, IQ imbalance.

EGPRS LA

Query

Integrity indicator

RMS Error Vector Magnitude

  • Range: 0 % to 100 % and 9.91 E+37 (NAN)
  • Resolution: 0.01 %

Peak Error Vector Magnitude

  • Range: 0 % to 100 % and 9.91 E+37 (NAN)
  • Resolution: 0.01 %

95th Percentile Error Vector Magnitude

  • Range: 0 % to 100 % and 9.91 E+37 (NAN)
  • Resolution: 0.01 %

Frequency Error

  • Range: -9999 Hz to +9999 Hz and 9.91 E+37 (NAN)
  • Resolution: 0.01 Hz

Origin Offset Suppression

  • Range: -70 dB to 0 dB and 9.91 E+37 (NAN)
  • Resolution: 0.01 dB

RMS Phase Error

  • Range: 0 to 180 degrees and 9.91 E+37 (NAN)
  • Resolution: 0.01 degrees

Peak Phase Error

  • Range: 0 to 180 degrees and 9.91 E+37 (NAN)
  • Resolution: 0.01 degrees

RMS Magnitude Error

  • Range: 0 to 100 % and 9.91 E+37 (NAN)
  • Resolution: 0.01 %

Peak Magnitude Error

  • Range: 0 to 100 % and 9.91 E+37 (NAN)
  • Resolution: 0.01 %

Amplitude Droop

  • Range: -20 dB to +20 dB and 9.91 E+37 (NAN)
  • Resolution: 0.01 dB

IQ Imbalance

  • Range: 0 dB to +100 dB and 9.91 E+37 (NAN)
  • Resolution: 0.01 dB

AM-PM Timing Offset

  • Range: -5000ns to 5000ns and 9.91 E+37 (NAN)
  • Resolution: 1ns
Requirements GSM/GPRS/
EGPRS TA

Revision: A.03 and above

Revision: A.11 and above adds AM-PM Timing Offset

GSM/GPRS/ EGPRS LA

Revision: C.03 and above

READ:EMACcuracy[:ALL]:ETSI?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

GSM/GPRS LA

This command is not applicable to the GSM/GPRS LA.

EGPRS TA

Queries (initiates and fetches) the ETSI specified 8PSK multislot modulation accuracy results. The query returns integrity indicator, RMS error vector magnitude (EVM), peak EVM, 95th percentile EVM, frequency error, and origin offset suppression.

EGPRS LA

Query

Integrity indicator

RMS Error Vector Magnitude

  • Range: 0 % to 100 % and 9.91 E+37 (NAN)
  • Resolution: 0.01 %

Peak Error Vector Magnitude

  • Range: 0 % to 100 % and 9.91 E+37 (NAN)
  • Resolution: 0.01 %

95th Percentile Error Vector Magnitude

  • Range: 0 % to 100 % and 9.91 E+37 (NAN)
  • Resolution: 0.01 %

Frequency Error

  • Range: -9999 Hz to +9999 Hz and 9.91 E+37 (NAN)
  • Resolution: 0.01 Hz

Origin Offset Suppression

  • Range: -70 dB to 0 dB and 9.91 E+37 (NAN)
  • Resolution: 0.01 dB
Requirements GSM/GPRS/
EGPRS TA

Revision: A.03 and above

GSM/GPRS/ EGPRS LA

Revision: C.03 and above

READ:ETXPower[:ALL]?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

GSM/GPRS LA

This command is not applicable to the GSM/GPRS LA.

EGPRS TA

Queries (initiates and fetches) one EGPRS TX power measurement as a sequential operation.

Returns Integrity Indicator (see Integrity Indicator ), average burst power, and average estimated carrier power.

When the selected modulation format is set to GMSK, Burst Power and Carrier Power measurements are equivalent so both results return the same value.

EGPRS LA

Query

Integrity indicator

Burst power (average)

  • Range: -100 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB

Estimated carrier power (average)

  • Range: -100 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB
Requirements GSM/GPRS/
EGPRS TA

Revision: A.03 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:FBERror[:ALL]?

Function

GSM

Queries (initiates and fetches) one fast bit error measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio, and Fast Bit Error Count using mobile station burst-by-burst looback (type C loopback). The FETCh command should be used to obtain other measurement results. See FETCh:BERRor .

GSM/GPRS LA

EGPRS LA

GPRS TA

This command is not applicable to GPRS.

EGPRS TA

This command is not applicable to EGPRS.

Query

Integrity indicator

Bits tested

  • Range: 0 to (RX Fast BER bits to test + 455) and 9.91E+37 (NAN)
  • Resolution: 1

Bit error ratio

  • Range: 0 to 100 and 9.91E+37 (NAN)
  • Resolution: 1

Fast bit error count

  • Range: 0 to (RX Fast BER bits to test + 455) and 9.91E+37 (NAN)
  • Resolution: 1

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:FFERate[:ALL]?

Function

GSM/GPRS LA

Queries (initiates and fetches) one frame erasure rate on FACCH full rate speech measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , Samples, Frame Erasure Ratio, and Count of Retransmissions. The FETCh command should be used to obtain other measurement results. See FETCh:FFERate .

EGPRS LA

GSM TA

This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

Query

Integrity indicator

Samples

  • Range: 0 to 999999 and 9.91E+37 (NAN)
  • Resolution: 1

Frame erasure ratio

  • Range: 0 to 100% and 9.91E+37 (NAN)
  • Resolution: 0.001

Frame erasure count

  • Range: 0 to 999999 and 9.91E+37 (NAN)
  • Resolution: 1

Requirements

GSM/GPRS/ EGPRS LA

Revision: C.03 and above

READ:FSTability[:ALL]?

Function

GSM TA

Initiates and fetches a frequency stability measurement as a sequential operation.

Measurement results are returned in the following order: integrity, worst-case frequency error, average frequency.

GPRS TA

EGPRS TA

GSM/GPRS LA

EGPRS LA

Function

Initiates and fetches a frequency stability measurement as a sequential operation.

Measurement results are returned in the following order: integrity, worst-case frequency error, average frequency.

Query

Integrity

Worst-case frequency error

  • Range: -500 to 500 parts per million (ppm), 9.91 E+37
  • Resolution: 0.01

Average frequency

  • Range: 100 E+6 to 3 E+9 Hz, 9.91 E+37
  • Resolution: 1 Hz
Requirements GSM/GPRS/
EGPRS TA

Revision: A.04 and above

GSM/GPRS/ EGPRS LA

Revision: D.01 and above

READ:GBERror[:ALL]?

Function

GSM TA

This command is not applicable to GSM.

GPRS TA

Queries (initiates and fetches) one bit error measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio, and Bit Error Count. The FETCh command should be used to obtain other measurement results. See FETCh:GBERror .

EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Integrity indicator

Bits tested

  • Range: 0 to 999,427 and 9.91E+37 (NAN)
  • Resolution: 1

Bit error ratio

  • Range: 0 to 100 and 9.91E+37 (NAN)
  • Resolution: 1

Bit error count

  • Range: 0 to 999,427 and 9.91E+37 (NAN)
  • Resolution: 1
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:GPESquality[:ALL]?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA

Initiates and fetches the Perceptual Evaluation of Speech Quality Measurement as a sequential operation.

Measurement results are returned in the following order: Integrity, Uplink PESQ Score, Downlink PESQ Score,PESQ Uplink Headroom, PESQ Downlink Headroom.

EGPRS LA

Query

Integrity

  • Range: 0 to 31
  • Resolution: 1

Uplink PESQ Score

  • Range: -0.5 to 4.5, 9.91 E+37
  • Resolution: 0.01

Downlink PESQ Score

  • Range: -0.5 to 4.5, 9.91 E+37
  • Resolution: 0.01

PESQ Uplink Headroom

  • Range: 0.0 to 100.0 dB, 9.91 E+37
  • Resolution: 0.1 dB

PESQ Downlink Headroom

  • Range: 0.0 to 100.0 dB, 9.91 E+37
  • Resolution: 0.1 dB

Requirements GSM/GPRS/ EGPRS LA

Revision: H.00.xx and above

READ:IFERror[:ALL]?

Function

GSM TA

This command is not applicable to the GSM TA.

GPRS TA

This command is not applicable to the GPRS TA.

EGPRS TA

This command is not applicable to the EGPRS TA.

GSM/GPRS LA

Queries (initiates and fetches) one bit error measurement as a sequential operation.

Returns the results in the following order: integrity, speech frames measured, frame error ratio, and frame error count.

EGPRS LA

Query

Integrity indicator

Number of speech frames tested

  • Range: 1 to 900000 or 9.91e+37 (NAN)
  • Resolution: 1

Frame Error Ratio

  • Range: 0 to 100 or 9.91e+37 (NAN)
  • Resolution: .001

Frame Error Count

  • Range: 0 to 900000 or 9.91e+37 (NAN)
  • Resolution: 1
Requirements GSM/GPRS/ EGPRS LA

Revision: D.01 and above

READ:IQTuning[:ALL]?

Function

GSM TA

Queries (initiates and fetches) the I/Q Tuning measurement results. Query returns the integrity indicator and the relative power level at the following offset frequencies: carrier frequency, 䕧.7083 kHz, 𫏯.417 kHz, 𫐳.125 kHz, 𫑶.833 kHz. The spur measurement result is also returned.

The FETCh command should be used to return other measurement results. See FETCh:IQTuning .

GPRS TA

EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Integrity indicator

Signal level relative to the desired signal at 9 different frequencies

  • Range: -100 to +100 dB and 9.91 E+37 (NAN)
  • Resolution: 0.01 dB

The order of the signal level results are:

  • -270.833 kHz
  • -203.125 kHz
  • -135.417 kHz
  • -67.7083 kHz
  • carrier frequency
  • +67.7083 kHz
  • +135.417 kHz
  • +203.125 kHz
  • +270.833 kHz

Relative power of the spur frequency:

  • Range: -100 to +100 dB and 9.91E+37 (NAN)
  • Resolution: 0.01 dB

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:MTAudio[:ALL]?

Function

GSM TA

Queries (initiates and fetches) the Multi-Tone Audio measurement results. Query returns the integrity indicator and a comma separated list of RMS audio levels for the 20 audio tones.

The FETCh command should be used to return other measurement results. See FETCh:MTAudio[:ALL]? .

GSM/GPRS LA

EGPRS LA

GPRS TA

This command is not applicable to GPRS.

EGPRS TA

This command is not applicable to EGPRS.

Query

Integrity indicator

Audio level

  • Range: -100 to +100 dB and 9.91 E+37 (NAN)
  • Resolution: 0.1 dB

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:ORFSpectrum[:ALL]?

Function

GSM TA

Queries (initiates and fetches) one output RF spectrum measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , TX Power, Output RF Spectrum due to Switching (Max), 30 kHz Bandwidth Power, and Output RF Spectrum due to Modulation (Average). The FETCh command should be used to obtain other measurement results. See FETCh:ORFSpectrum .

GPRS TA

EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Integrity indicator

TX power

  • Range: -100 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB

Output RFspectrum due to switching (Max)

  • Range: 0 to 8 comma separated values -100 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB

30 kHz bandwidth power

  • Range: -100 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB

Output RF spectrum due to modulation (average)

  • Range: 0 to 22 comma separated values -200 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:PCALibration[:ALL]?

Function

GSM TA

This command initiates the Phase and Amplitude versus Time measurement and fetches the results when the measurement is complete.

This query is only applicable when the waveform type is DISCrete and the result type is PCAL or BOTH . The command to set the waveform type is SETup:PCALibration:WAVeform:TYPE , and the command to set the result type is SETup:PCALibration:RESult:TYPE .

If the waveform type is CONTinuous or the waveform type is DIScrete and the result type is SAMPle , only the measurement integrity result is valid .When the result type is set to PCAL or BOTH other results are reported as single NaN results.

The values returned by this query are a single integrity result for the measurement followed by a comma separated list of up to 512 measured power values, followed by a comma separated list of up to 512 measured phase values, followed by a comma separated list of up to 512 frequency error results.

The first measured power value is the absolute power level and all subsequent power values are relative to the absolute power. The first phase value is 0° and all subsequent values are phase values relative to the 0° reference. The first frequency value is the absolute frequency, and all subsequent values are relative to the absolute frequency.

GPRS TA

EGPRS TA

GSM/GPRS LA

EGPRS LA

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.06 and above with the required feature license

GSM/GPRS/
EGPRS LA

Revision: D.03 and above

READ:PFERror[:ALL]?

Function

GSM TA

Queries (initiates and fetches) one Phase and Frequency Error measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , RMS Phase Error (Max), Peak Phase Error (Max), Frequency Error (Worst). The FETCh command should be used to obtain other measurement results. See FETCh:PFERror .

Worst frequency error (negative or positive) is the value furthest from zero.

GPRS TA

EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Integrity indicator

rms phase error (max)

  • Range: 0 to 180 degrees and 9.91E+37 (NAN)
  • Resolution: 0.01 dB

Peak phase error (max)

  • Range: 0 to 180 degrees and 9.91E+37 (NAN)
  • Resolution: 0.01 degrees

Frequency error (worst)

  • Range: -750 kHz to +750 kHz and 9.91E+37 (NAN)
  • Resolution: 0.01 Hz
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:PFERror[:ALL]:FAIL?

Function

GSM

Queries (initiates and fetches) one Phase and Frequency Error measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , RMS Phase Error pass/fail indicator, Peak Phase Error pass/fail indicator, Frequency Error pass/fail indicator, and the number of measurements taken. The number of measurements taken may be of interest to you if you are using the confidence level feature. For more information on using confidence levels refer to Confidence Levels .

The FETCh command should be used to obtain other measurement results. See FETCh:PFERror .

Worst frequency error (negative or positive) is the value furthest from zero.

GSM/GPRS LA

EGPRS LA

GPRS TA

EGPRS TA

Query

Integrity indicator

RMS phase error pass/fail indicator

  • Range: 0|1

Peak phase error pass/fail indicator

  • Range: 0|1

Frequency error pass/fail indicator

  • Range: 0|1

Number of measurements taken

  • Range: 0 to 999 and 9.91 E+37 (NAN)
  • Resolution: 1

Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:PVTime[:ALL]?

Function

GSM TA

Queries (initiates and fetches) one power versus time measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , Mask pass/fail, power versus time transmit power and up to 12 power versus time offset (max) results. The FETCh command should be used to obtain other measurement results. See FETCh:PVTime .

GSM/GPRS LA

EGPRS LA

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the GPRS Test Application.

Query

Integrity indicator

Mask pass/fail

  • Range: 0|1 and 9.91E+37 (NAN)

Power versus time transmit power

  • Range: -100 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB

Power versus time offset (max)

  • Range: Up to 12 comma-separated power versus time values returned with max power = -100 dBc to +100 dBc (relative to power versus time carrier power) and 9.91E+37 (NAN)
  • Resolution: 0.01 dB
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ[:BURSt[1]]:PVTime[:ALL]?

READ:BURSt2|3|4|5:PVTime[:ALL]?

Function

GSM TA This command is not applicable for GSM.

GPRS TA

Queries (initiates and fetches) one power versus time measurement as a sequential operation for the burst in the multislot configuration that you specify.

Returns Integrity Indicator see Integrity Indicator , Mask pass/fail, power versus time transmit power and up to 12 power versus time offset (max) results. The FETCh command should be used to obtain other measurement results. See FETCh:PVTime .

EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Integrity indicator

Mask pass/fail

  • Range: 0|1 and 9.91E+37 (NAN)

Power versus time transmit power

  • Range: -100 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB

Power versus time offset (max)

  • Range: Up to 12 comma-separated power versus time values returned with max power = -100 dBc to +100 dBc (relative to power versus time carrier power) and 9.91E+37 (NAN)
  • Resolution: 0.01 dB
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

Revision: A.08 adds Burst 3 and 4

Revision: A.09 adds Burst 5

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

Revision: E.02 adds Burst 3 and 4

Revision: F.01 adds Burst 5

READ:SBERror[:ALL]?

Function

GSM TA

This command is not applicable to GSM TA.

GPRS TA

This command is not applicable to GPRS TA.

GSM/GPRS LA

This command is not applicable to the GSM/GPRS LA.

EGPRS TA

Queries (initiates and fetches) one bit error measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , Bits Tested, Bit Error Ratio, and Bit Error Count. The FETCh command should be used to obtain other measurement results. See FETCh:SBERror .

EGPRS LA

Query

Integrity indicator

Bits tested

  • Range: 0 to 999,427 and 9.91E+37 (NAN)
  • Resolution: 1

Bit error ratio

  • Range: 0 to 100 and 9.91E+37 (NAN)
  • Resolution: 1

Bit error count

  • Range: 0 to 999,427 and 9.91E+37 (NAN)
  • Resolution: 1
Requirements GSM/GPRS/
EGPRS TA

Revision: A.03 and above

GSM/GPRS/ EGPRS LA

Revision: C.03 and above

READ:SFERate[:ALL]?

Function

GSM/GPRS LA

Queries (initiates and fetches) one Repeated SACCH Frame Erasure Rate (FER) measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator , Samples, Frame Erasure Ratio, and Frame Erasure Count. The FETCh command should be used to obtain other measurement results. See FETCh:SFERate[:ALL]? .

EGPRS LA

GSM TA

This command is not applicable to the GSM Test Application.

GPRS TA

This command is not applicable to the GPRS Test Application.

EGPRS TA

This command is not applicable to the EGPRS Test Application.

Query

Integrity indicator

Samples

  • Range: 0 to 999999 and 9.91E+37 (NAN)
  • Resolution: 1

Frame erasure ratio

  • Range: 0 to 100% and 9.91E+37 (NAN)
  • Resolution: 0.001

Frame erasure count

  • Range: 0 to 999999 and 9.91E+37 (NAN)
  • Resolution: 1

Requirements

GSM/GPRS/ EGPRS LA

Revision: F.00.37 and above

READ:SMONitor:TRACe?

Function

GSM TA

Queries (initiates and fetches) one spectrum monitor measurement as a sequential operation.

Returns a comma separated list of 401 points representing the amplitude results of the trace data.

GPRS TA

EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Range:

  • For spans of 125 kHz and 500 kHz

    • frequency of point: within the current span (relative to the center frequency)
    • amplitude of point: -50 to +55 dB
  • For all other spans

    • frequency of point: within the current span (relative to the center frequency)
    • amplitude of point: (reference level - 60 dB) to +55 dB
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above

READ:TXPower[:ALL]?

Function

GSM TA

Queries (initiates and fetches) one TX power measurement as a sequential operation.

Returns Integrity Indicator see Integrity Indicator and transmit power (average). The FETCh command should be used to obtain other measurement results. See FETCh:TXPower .

GPRS TA

GSM/GPRS LA

EGPRS LA

EGPRS TA

This command is not applicable to the EGPRS Test Application.

Query

Integrity indicator

Transmit power (average)

  • Range: -100 to +100 dBm and 9.91E+37 (NAN)
  • Resolution: 0.01 dB
Requirements GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/ EGPRS LA

Revision: C.01 and above