Last updated: December 3, 2008
Sets/queries which channel (RACH, TCH or PDTCH) is measured when the operating mode is GSM BCH, GPRS BCH or EGPRS BCH. See Measurement Channel in BCH Only Mode . |
||
GPRS TA | ||
Range: RACH | TCH | PDTCh | ||
*RST setting | RACH | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"RFANalyzer:CONTrol:BTESt:CHANnel TCH" ! Sets the Measurement Channel in BCH Only Mode to TCH. |
Sets/queries whether the test set's receiver is set to automatic (AUTO ON) or manual (AUTO OFF) measurement frequency control. See Receiver Control . |
||
GPRS TA | ||
Range: 1 | ON | 0 | OFF | ||
*RST setting | 1 | ON | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"RFANalyzer:CONTrol:MEASurement:FREQuency:AUTO OFF" ! Enables manual control of the measurement receiver's frequency. |
Sets/queries whether the test set receiver's expected power setting is set to automatic (AUTO ON) or manual (AUTO OFF) power control. See Receiver Control . |
||
*RST setting | 1 | ON | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"RFANalyzer:CONTrol:POWer:AUTO OFF" |
Sets/queries whether the test set's demodulation receiver is set to automatic (AUTO ON) or manual (AUTO OFF) uplink frequency control. See Receiver Control . |
||
*RST setting | 1 | ON | |
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"RFANalyzer:CONTrol:UPLink:FREQuency:AUTO OFF" ! The test set's demodulation receiver is set to manual uplink frequency control. |
Sets/queries the power level in DBM that the mobile station is expected to transmit in CW mode. The units DBM are optional. The test set will set up its input signal path to measure this power level. See Expected Power Control . |
||
Range: -60 to +53 dBm, after the Amplitude Offset (optional) has been factored in. see Amplitude Offset . |
||
Range: -60 to +53 dBm, after the Amplitude Offset (optional) has been factored in. see Amplitude Offset . |
||
*RST setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"RFANalyzer:CW:EXPected:POWer -20 DBM" ! Sets the expected power transmit level to -20 dBm. |
This command sets/queries the power level in dBm that the test set's receiver is expecting the mobile station uplink burst to transmit at for the active (that is the selected) format. This setting applies when the Multislot Configuration setting allows the number of uplink bursts that you wish to set, or Uplink Test Sequence Burst Count (while in FastTune operating mode) is at least as high as the burst power you wish to set.
Bursts 5 through 8 only apply when the operating mode is set to |
||
Range: -60 dBm to +53 dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset . |
||
Range: -60 dBm to +53 dBm, after the Amplitude Offset (optional) has been included, see Amplitude Offset . |
||
*RST setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA |
Revision D.01 adds Burst3 and Burst4 Revision E.01 adds Burst 5 through 7. |
|
OUTPUT 714;"RFANalyzer:MANual:POWer:BURSt 7" ! Sets the test set expected burst power of the first burst level to 7 dBm. |