This command sets/queries the center frequency for the 100 Hz bandpass filter applied to Decoded Audio measurements. This command sets the count state to ON. The units (HZ|KHZ) are optional, if no units are specified then units default to KHZ. see Decoded Audio Measurement Description | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Setting | ||
*RST Setting | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETUP:DAUDIO:FILTER:SFREQUENCY 2.2KHZ" ! This is a complex command that sets the value and the state to on. |
This command sets/queries the center frequency for the 100 Hz bandpass filter applied to Decoded Audio measurements. The units (HZ|KHZ) are optional, if no units are specified then units default to KHZ. see Decoded Audio Measurement Description | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Setting | ||
*RST Setting | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"DAUDIO:FILTER:FREQUENCY 217HZ" ! Sets bandpass filter frequency. |
This command selects/queries the Decoded Audio bandpass filter state. see Decoded Audio Measurement Description | ||
This command is not applicable to GPRS. | ||
This command is not applicable to EGPRS. | ||
Setting | Range: 1|ON |0|OFF | |
Range: 1|0 | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"ABORT:ALL" ! Aborts all active measurements in progress. |
||
OUTPUT 714;"SETUP:DAUDIO:FILTER:STATE OFF" ! Sets bandpass filter state to off. |