This command is not applicable to GSM. | ||
This command is not applicable to GPRS. | ||
This command is not applicable to the GSM/GPRS LA. | ||
This command selects/queries the trigger source for EGPRS modulation accuracy measurements. See Triggering of Measurements . |
||
Setting | ||
*RST Setting | ||
Requirements |
GSM/GPRS/ EGPRS TA |
|
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:EMACcuracy:TRIGger:SOURce AUTO" ! Sets trigger source to automatic. |