STATus:OPERation
Last updated: December 3, 2008
GPIB Command Conventions
STATus:OPERation Condition Register Bit Assignment
The OPERation status register set contains bits which give an indication of conditions that are part of the test set's normal operation.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Processing SYSTem:SYNChronized Command
|
This condition bit is "pulsed" by the SYSTem:SYNChronized command. This allows the status system to indicate that the input buffer is synchronized to the point where this command is parsed and that all prior sequential commands are completed and all prior overlapped commands have started.
|
11
|
2048
|
Reserved for future use |
This bit is always 0. |
10
|
1024
|
CALL Summary
|
This bit is the summary bit for the STATus:OPERation:CALL register.
|
9
|
512
|
NMRReady (New Measurement Result Ready) Summary
|
This bit is the summary bit for the STATus:OPERation:NMRReady register.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
Reserved for future use.
|
This bit is always 0.
|
6
|
64
|
Reserved for future use.
|
This bit is always 0.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
Reserved for future use.
|
This bit is always 0.
|
3
|
8
|
Reserved for future use.
|
This bit is always 0.
|
2
|
4
|
Reserved for future use.
|
This bit is always 0.
|
1
|
2
|
Reserved for future use.
|
This bit is always 0.
|
0
|
1
|
Extension Bit
|
This bit is always 0.
|
Program Examples - STATus:OPERation
OUTPUT 714;"STATUS:OPERATION:EVENT?" !Queries and clears the Operation
!Event Register
OUTPUT 714;"STATUS:OPERATION:CONDITION?" !Queries and clears the Operation
!Condition Register
OUTPUT 714;"STATUS:OPERATION:ENABLE 1024" !Sets the Operation
!Enable
!Register for bit 10
OUTPUT 714;"STATUS:OPERATION:NTRANSITION 2" !Sets the Operation
!Negative Transition
!Filter Register for bit 1
OUTPUT 714;"STATUS:OPERATION:PTRANSITION 2" !Sets the Operation
!Positive Tranasition
!Filter Register for bit 1
STATus:OPERation:CALL Condition Register Bit Assignment
The STATus:OPERation:CALL register bits are used to indicate status of processes that occur during normal call processing operations.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
GPRS Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:GPRS register.
|
11
|
2048
|
WCDMa Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:WCDMa register.
|
10
|
1024
|
FDD Summary bit |
This bit is the summary bit for the STATus:OPERation:CALL:FDD register.
|
9
|
512
|
TA2000 Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:TA2000 register.
|
8
|
256
|
CDMA Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:CDMA register.
|
7
|
128
|
DIGital2000 Summary bit.
|
This bit is the summary bit for the STATus:OPERation:CALL:DIGital2000 register.
|
6
|
64
|
DIGital95 Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:DIGital95 register.
|
5
|
32
|
TA136 Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:TA136 register.
|
4
|
16
|
DIGital136 Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:DIGital136 register.
|
3
|
8
|
AMPS Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:AMPS register.
|
2
|
4
|
GSM Summary bit |
This bit is the summary bit for the STATus:OPERation:CALL:GSM register. |
1
|
2
|
COMMon Summary bit
|
This bit is the summary bit for the STATus:OPERation:CALL:COMMon register.
|
0
|
1
|
Extension Bit |
This bit is always 0.
|
Program Examples - STATus:OPERation:CALL
OUTPUT 714;"STATUS:OPERATION:CALL:EVENT?" !Queries and clears the Operation Call Event
!Register
OUTPUT 714;"STATUS:OPERATION:CALL:CONDITION?" !Queries and clears the Operation Call
!Condition Register
OUTPUT 714;"STATUS:OPERATION:CALL:ENABLE 4" !Sets the Operation Call Enable
!Register for bit 2
OUTPUT 714;"STATUS:OPERATION:CALL:NTR 4" !Sets the Negative Transition Filter
!Register for bit 2
OUTPUT 714;"STATUS:OPERATION:CALL:PTR 256" !Sets the Positive Transition Filter
!Register for bit 8
STATus:OPERation:CALL:COMMon Condition Register Bit Assignment
The STATus:OPERation:CALL:COMMon register bits are used to indicate status of processes that occur during normal call processing operations.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Data Summary
|
This bit is the summary bit for the STATus:QUEStionable:CALL:GSM:DATA register. |
13
|
8192
|
Call Control Status Access Probe |
This bit is a 1 when the test set is in the call control status access probe state.
|
12
|
4096
|
Call Control Status Set Up Request
|
This bit is a 1 when the test set is in the call control status set up request state.
|
11
|
2048
|
Call Control Status Releasing
|
This bit is a 1 when the test set is in the call control status releasing state.
|
10
|
1024
|
Call Control Status Paging
|
This bit is a 1 when the test set is in the call control status paging state.
|
9
|
512
|
Registering (BS initiated)
|
This bit is set to a 1 when the Base Station initiates registration.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
BS Originating
|
This bit is a 1 when:
|
6
|
64
|
Call Control Status Changing
|
This bit is set to a 1 when the call control status change detector has been armed.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
Reserved for future use.
|
This bit is always 0.
|
3
|
8
|
Call Control Status Alerting
|
This bit is a 1 when the test set is in the call alerting state (ringing).
|
2
|
4
|
Call Control Status Connected
|
This bit is a 1 when the test set is in the call connected state.
|
1
|
2
|
Call Control Status Idle
|
This bit is a 1 when the test set is in the call idle state.
|
0
|
1
|
Extension Bit
|
This bit is always 0.
|
Program Examples STATus:OPERation:CALL:COMMon
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:EVENT?" !Queries and clears the Operation
!Call
!Common Event Register
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:CONDITION?" !Queries and clears the Operation
!Call
!Common Condition Register
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:ENABLE 1024" !Sets the Operation
!Call
!Common Enable
!Register for bit 10
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:NTRANSITION 2" !Sets the Operation
!Call
!Common Negative Transition
!Filter Register for bit 1
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:PTRANSITION 2" !Set the Operation
!Call
!Common Positive Transition
!Filter Register for bit 1
STATus:OPERation:CALL:COMMon:DAINterface Condition Register Bit Assignment
The STATus:OPERation:CALL:COMMon:DAINterface register bits are used to indicate status of processes that occur during digital audio interface test processing operations.
Bit Number
|
Bit Name
|
Description
|
15
|
Not Used.
|
This bit is always 0.
|
14-5
|
Reserved for future use. |
These bits are always 0. |
4
|
Ready to play |
This bit is set to 1 then cleared to 0 when a file has been successfully uploaded.
|
3
|
Playing state |
This bit is set to 1 while playing a digital audio file.
|
2
|
Record buffer filled
|
This bit is set to 1 then cleared to 0 when recording was terminated by the record buffer being filled.
|
1
|
Recording state
|
This bit is set to 1 while recording a digital audio file.
|
0
|
Extension Bit
|
Reserved for future use.
|
Program Examples STATus:OPERation:CALL:COMMon:DAINterface
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DAIN:EVENT?" !Queries and clears the Operation
!Call Common DAI Interface
!Event Register
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DAIN:CONDITION?" !Queries and clears the Operation
!Call Common DAI Interface
!Condition Register
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DAIN:ENABLE 8" !Sets the Operation Call Common
!DAI Interface Enable Register
!for bit 3
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DAIN:NTRANSITION 2" !Sets the Operation Call Common
!DAI Interface Negative Transition
!Filter Register for bit 1
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DAIN:PTRANSITION 2" !Set the Operation Call Common
!DAI Interface Positive Transition
!Filter Register for bit 1
STATus:OPERation:CALL:COMMon:DATA Condition Register Bit Assignment
The STATus:OPERation:CALL:COMMon:DATA register bits are used to indicate status of processes that occur during normal data connection processing operations.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Ping active. |
This bit is a 1 when a Ping session is active.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
Data Connection Status Suspended
|
This bit is a 1 when the status is Suspended, zero when not Suspended. |
10
|
1024
|
Data Connection Status Dormant
|
This bit is a 1 when the Status is Dormant, zero when not Dormant. |
9
|
512
|
Data Connection Status Session Open
|
This bit is a 1 when the Status Session is Open, zero when Closed.
|
8
|
256
|
PDP Active state
|
This bit is a 1 when the PDP is active, zero when inactive.
|
7
|
128
|
Starting Data Connection
|
This bit is a 1 when:
|
6
|
64
|
Data Connection Status Changing
|
This bit is set to a 1 when the data connection status change detector has been armed.
|
5
|
32
|
Data Connection Status Off |
This bit is set to 1 when the test set is in the call control status handover/handoff state. |
4
|
16
|
Data Connection Status Data Connected |
This bit is set to 1 when:
-
data connection status data is in the connected state.
-
a circuit switched data (CSD) connection is active.
|
3
|
8
|
Data Connection Status Transferring
|
This bit is a 1 when the data connection status is Transferring.
|
2
|
4
|
Data Connection Status Attached
|
This bit is a 1 when the data connection status is Attached.
|
1
|
2
|
Data Connection Status Idle
|
This bit is a 1 when the data connection status is Idle.
|
0
|
1
|
Extension Bit
|
This bit is always 0.
|
Program Examples STATus:OPERation:CALL:COMMon:DATA
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DATA:EVENT?" !Queries and clears the Operation
!Call Common Data Event Register
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DATA:CONDITION?" !Queries and clears the Operation
!Call Common Data Condition
!Register
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DATA:ENABLE 128" !Sets the Operation Call Common
!Data Enable Register for bit 7
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DATA:NTRANSITION 2" !Sets the Operation Call Common
!Data Negative Transition Filter
!Register for bit 1
OUTPUT 714;"STATUS:OPERATION:CALL:COMMON:DATA:PTRANSITION 2" !Set the Operation Call Common
!Data Positive Transition Filter
!Register for bit 1
STATus:OPERation:CALL:GSM Condition Register Bit Assignment
The STATus:OPERation:CALL:GSM register bits are used to indicate status of processes that occur during normal GSM call processing operations. These register bits are not applicable to GPRS.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
RRLP Measurement Position Request Received.
|
If message queuing is "OFF", the CONDition bit moves from 0 to 1 and back to 0 when the event takes place. If message queuing is "ON", the CONDition bit is set to 1 and remains there until the test set is informed by the controller that all received messages have been read. |
13
|
8192
|
RRLP Assistance Data Ack Received.
|
If message queuing is "OFF", the CONDition bit moves from 0 to 1 and back to 0 when the event takes place. If message queuing is "ON", the CONDition bit is set to 1 and remains there until the test set is informed by the controller that all received messages have been read. |
12
|
4096
|
RRLP Pipe Data Received.
|
If message queuing is "OFF", the CONDition bit moves from 0 to 1 and back to 0 when the event takes place. If message queuing is "ON", the CONDition bit is set to 1 and remains there until the test set is informed by the controller that all received messages have been read.
|
11
|
2048
|
Reserved for future use.
|
This bit is always 0.
|
10
|
1024
|
Reserved for future use.
|
This bit is always 0.
|
9
|
512
|
Reserved for future use.
|
This bit is always 0.
|
8
|
256
|
BS Disconnecting
|
This bit is a 1 when:
|
7
|
128
|
BS Originating
|
This bit is a 1 when:
|
6
|
64
|
Call Control Status Changing
|
This bit is set to a 1 when the call control status change detector has been armed.
|
5
|
32
|
TCH Assignment in Progress
|
This bit is a 1 when:
-
The channel assignment is successfully completed (when a call is established).
-
The test set notes a change in the TCH ARFCN, cell band, TCH timeslot, or mobile station timing advance.
-
An error message is generated.
|
4
|
16
|
BCH Changing
|
This bit is a 1 when:
|
3
|
8
|
Call Control Status Alerting
|
This bit is a 1 when the test set is in the call alerting state (ringing).
|
2
|
4
|
Call Control Status Connected
|
This bit is a 1 when:
-
the test set is in the call connected state.
-
a circuit switched data (CSD) connection is active.
|
1
|
2
|
Call Control Status Idle
|
This bit is a 1 when the test set is in the call idle state.
|
0
|
1
|
Extension Bit
|
This bit is always 0.
|
Program Examples - STATus:OPERation:CALL:GSM
OUTPUT 714;"STATUS:OPERATION:CALL:GSM:EVENT?" !Queries and clears the Operation
!Call GSM Event Register
OUTPUT 714;"STATUS:OPERATION:CALL:GSM:CONDITION?" !Queries and clears the Operation
!Call GSM Condition Register
OUTPUT 714;"STATUS:OPERATION:CALL:GSM:ENABLE 1024" !Sets the Operation
!Call GSM Enable
!Register for bit 10
OUTPUT 714;"STATUS:OPERATION:CALL:GSM:NTRANSITION 2" !Sets the Operation
!Call GSM Negative Transition
!Filter Register for bit 1
OUTPUT 714;"STATUS:OPERATION:CALL:GSM:PTRANSITION 2" !Sets the Operation
!Call GSM Positive Tranasition
!Filter Register for bit 1
STATus:OPERation:FEATures Register Bit Assignments
The STATus:OPERation:FEATures register bits are used to access miscellaneous Features Registers.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
Reserved for future use.
|
This bit is always 0.
|
10
|
1024
|
Reserved for future use.
|
This bit is always 0.
|
9
|
512
|
Reserved for future use.
|
This bit is always 0.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
Reserved for future use.
|
This bit is always 0.
|
6
|
64
|
Reserved for future use.
|
This bit is always 0.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
Reserved for future use.
|
This bit is always 0.
|
3
|
8
|
Reserved for future use.
|
This bit is always 0.
|
2
|
4
|
Reserved for future use.
|
This bit is always 0.
|
1
|
2
|
COMMon Summary Bit |
This bit is the summary bit for the STATus:OPERation:FEATures:COMMon register. (see
STATus:OPERation:FEATures:COMMon Register Bit Assignments
) |
0
|
1
|
Extension Bit |
This bit is always 0.
|
Program Examples - STATus:OPERation:FEATures
OUTPUT 714;"STATUS:OPERATION:FEATures:EVENT?"
!Queries the Operation FEATures Event Register.
OUTPUT 714;"STATUS:OPERATION:FEATures:CONDITION?"
!Queries the Operation FEATures Condition Register.
OUTPUT 714;"STATUS:OPERATION:FEATures:ENABLE 2"
!Sets Operation FEATures Enable register for bit 1.
OUTPUT 714;"STATUS:OPERATION:FEATures:NTR 2"
!Sets the Operation FEATures Negative Transition Register for bit 1.
OUTPUT 714;"STATUS:OPERATION:FEATures:PTR 4"
!Sets the Operation FEATures Positive Transition Register for bit 2
STATus:OPERation:FEATures:COMMon Register Bit Assignments
The STATus:OPERation:FEATures:COMMon register bits indicate the status of processes that occur during the operations.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
Reserved for future use.
|
This bit is always 0.
|
10
|
1024
|
Reserved for future use.
|
This bit is always 0.
|
9
|
512
|
Reserved for future use.
|
This bit is always 0.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
Reserved for future use.
|
This bit is always 0.
|
6
|
64
|
Reserved for future use.
|
This bit is always 0.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
Reserved for future use.
|
This bit is always 0.
|
3
|
8
|
Reserved for future use.
|
This bit is always 0.
|
2
|
4
|
Common Supplementary Services Summary bit.
|
This bit is the summary message bit for the STATus:OPERation:FEATures:COMMon:SSERvice register. (see
STATus:OPERation:FEATures:COMMon:SSERvice Register Bit Assignments
)
|
1
|
2
|
SMService Summary bit |
This bit is the summary message bit for the STATus:OPERation:FEATures:COMMon:SMService register. (see
STATus:OPERation:FEATures:COMMon:SMService Register Bit Assignments
)
|
0
|
1
|
Extension Bit |
This bit is always 0.
|
STATus:OPERation:FEATures:COMMon:SSERvice Register Bit Assignments
The STATus:OPERation:FEATures:COMMon:SService register bits indicate the status of processes that occur during SS operations.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
Reserved for future use.
|
This bit is always 0.
|
10
|
1024
|
Reserved for future use.
|
This bit is always 0.
|
9
|
512
|
Reserved for future use.
|
This bit is always 0.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
Reserved for future use.
|
This bit is always 0.
|
6
|
64
|
Reserved for future use.
|
This bit is always 0.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
Reserved for future use.
|
This bit is always 0.
|
3
|
8
|
Reserved for future use.
|
This bit is always 0.
|
2
|
4
|
Reserved for future use.
|
This bit is always 0.
|
1
|
2
|
SS Pipe data received.
|
If message queuing is "OFF", the CONDition bit moves from 0 to 1 and back to 0 when the event takes place. If message queuing is "ON", the CONDition bit is set to 1 and remains there until the test set is informed by the controller that all received messages have been read.
|
0
|
1
|
Extension Bit |
This bit is always 0.
|
Program Examples - STATus:OPERation:FEATures:COMMon:SSERvice
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SSERVICE:EVENT?"
!Queries the Operation FEATures Event Register.
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SSERVICE:CONDITION?"
!Queries the Operation FEATures Condition Register.
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SSERVICE:ENABLE 2"
!Sets Operation FEATures Enable register for bit 1.
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SSERVICE:NTRANSITION 2"
!Sets the Operation FEATures Negative Transition Register for bit 1.
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SSERVICE:PTRANSITION 4"
!Sets the Operation FEATures Positive Transition Register for bit
STATus:OPERation:FEATures:COMMon:SMService Register Bit Assignments
The STATus:OPERation:FEATures:COMMon:SMService register bits indicate the status of processes that occur during SMS operations.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Mobile-Originated SMS Message Queue Overflow
|
The CONDition bit moves from 0 to 1 and back to 0 when the event takes place. |
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
Reserved for future use.
|
This bit is always 0.
|
10
|
1024
|
Reserved for future use.
|
This bit is always 0.
|
9
|
512
|
Reserved for future use.
|
This bit is always 0.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
Mobile-Originated Message Received/Ready to be Returned
|
If message queuing is "OFF", the CONDition bit moves from 0 to 1 and back to 0 when the event takes place. If message queuing is "ON", the CONDition bit is set to 1 and remains there until the test set is informed by the controller that all received messages have been read. |
6
|
64
|
Reserved for future use.
|
This bit is always 0.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
Reserved for future use.
|
This bit is always 0.
|
3
|
8
|
Reserved for future use.
|
This bit is always 0.
|
2
|
4
|
Reserved for future use.
|
This bit is always 0.
|
1
|
2
|
Reserved for future use.
|
This bit is always 0.
|
0
|
1
|
Extension Bit |
This bit is always 0.
|
Program Examples - STATus:OPERation:FEATures:COMMon:SMService
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SMSERVICE:EVENT?"
!Queries the Operation FEATures Event Register.
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SMSERVICE:CONDITION?"
!Queries the Operation FEATures Condition Register.
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SMSERVICE:ENABLE 2"
!Sets Operation FEATures Enable register for bit 1.
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SMSERVICE:NTRANSITION 2"
!Sets the Operation FEATures Negative Transition Register for bit 1.
OUTPUT 714;"STATUS:OPERATION:FEATURES:COMMON:SMSERVICE:PTRANSITION 4"
!Sets the Operation FEATures Positive Transition Register for bit
STATus:OPERation:HARDware Register Bit Assignments
The STATus:OPERation:HARDware register bits indicate information about the test set's hardware during normal operation.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
Reserved for future use.
|
This bit is always 0.
|
10
|
1024
|
Reserved for future use.
|
This bit is always 0.
|
9
|
512
|
Reserved for future use.
|
This bit is always 0.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
Reserved for future use.
|
This bit is always 0.
|
6
|
64
|
Reserved for future use.
|
This bit is always 0.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
Reserved for future use.
|
This bit is always 0.
|
3
|
8
|
Reserved for future use.
|
This bit is always 0.
|
2
|
4
|
Reserved for future use.
|
This bit is always 0.
|
1
|
2
|
External Timebase in use
|
This bit is a 1 if a suitable external timebase is connected to the test set's 10 MHz REF IN connector on the rear panel of the test set.
|
0
|
1
|
Extension Bit |
This bit is always 0.
|
Program Examples - STATus:OPERation:HARDware
OUTPUT 714;"STATUS:OPERATION:HARDWARE:EVENT?" !Queries the Hardware Event Register.
OUTPUT 714;"STATUS:OPERATION:HARDWARE:CONDITION?" !Queries the Hardware Condition Register.
OUTPUT 714;"STATUS:OPERATION:HARDWARE:ENABLE 16" !Sets New Measurement Results Hardware for
bit 16.
OUTPUT 714;"STATUS:OPERATION:HARDWARE:NTR 2" !Sets the Hardware Negative Transition
!Register for bit 4.
OUTPUT 714;"STATUS:OPERATION:HARDWARE:PTR 4" !Sets the Hardware Positive Transition
!Register for bit 4.
STATus:OPERation:KEYPressed Register Bit Assignments
The STATus:OPERation:KEYpressed register bits indicate when a softkey on the test set's front panel has been pressed while the test set is in remote operating mode.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
F12 softkey |
This bit is a 1 when the F12 softkey has been pressed. |
10
|
1024
|
F11 softkey |
This bit is a 1 when the F11 softkey has been pressed. |
9
|
512
|
F10 softkey |
This bit is a 1 when the F10 softkey has been pressed. |
8
|
256
|
F9 softkey |
This bit is a 1 when the F9 softkey has been pressed. |
7
|
128
|
F8 softkey |
This bit is a 1 when the F8 softkey has been pressed. |
6
|
64
|
F7 softkey
|
This bit is a 1 when the F7 softkey has been pressed.
|
5
|
32
|
F6 softkey |
This bit is a 1 when the F6 softkey has been pressed.
|
4
|
16
|
F5 softkey
|
This bit is a 1 when the F5 softkey has been pressed. |
3
|
8
|
F4 softkey |
This bit is a 1 when the F4 softkey has been pressed.
|
2
|
4
|
F3 softkey |
This bit is a 1 when the F3 softkey has been pressed.
|
1
|
2
|
F2 softkey |
This bit is a 1 when the F2 softkey has been pressed.
|
0
|
1
|
F1 softkey |
This bit is a 1 when the F1 softkey has been pressed. |
Program Examples - STATus:OPERation:KEYPressed
OUTPUT 714;"STATUS:OPERATION:KEYPRESSED:EVENT?" !Queries the Keypressed Event Register.
STATus:OPERation:NMRReady Condition Register Bit Assignment
The STATus:OPERation:NMRReady register bits indicate when a measurement has been completed and new measurement results are available.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use. |
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
GPRS Summary bit
|
This bit is the summary bit for the STATus:OPERation:NMRReady:GPRS register.
|
11
|
2048
|
WCDMa Summary bit
|
This bit is the summary bit for the STATus:OPERation:NMRReady:WCDMa register.
|
10
|
1024
|
FDD Summary bit
|
This bit is the summary bit for the STATus:OPERation:NMRReady:FDD register.
|
9
|
512
|
TA2000 Summary bit
|
This bit is the summary bit for the STATus:OPERation:NMRReady:TA2000 register.
|
8
|
256
|
CDMA Summary bit
|
This bit is the summary bit for the STATus:OPERation:NMRReady:CDMA register.
|
7
|
128
|
DIGital2000 Summary bit
|
This bit is the summary bit for the STATus:OPERation:NMRReady:DIGital2000 register.
|
6
|
64
|
DIGital95 Summary bit
|
This bit is the summary bit for the STATus:OPERation:NMRReady:DIGital95 register.
|
5
|
32
|
TA136 Summary bit |
This bit is the summary bit for the STATus:OPERation:NMRReady:TA136 register.
|
4
|
16
|
DIGital136 Summary bit
|
This bit is the summary bit for the STATus:OPERation:NMRReady:DIGital136 register.
|
3
|
8
|
AMPS Summary bit |
This bit is the summary bit for the STATus:OPERation:NMRReady:AMPS register.
|
2
|
4
|
GSM Summary bit |
This bit is the summary bit for the STATus:OPERation:NMRReady:GSM register. |
1
|
2
|
COMMon Summary bit |
This bit is the summary bit for the STATus:OPERation:NMRReady:COMMon register.
|
0
|
1
|
Extension Bit |
This bit is always 0.
|
Program Examples - STATus:OPERation:NMRReady
OUTPUT 714;"STATUS:OPERATION:NMRREADY:EVENT?" !Queries and clears the New Measurement
!Results Ready Event Register
OUTPUT 714;"STATUS:OPERATION:NMRREADY:CONDITION?" !Queries and clears the New Measurement
!Results Ready
!Condition Register
OUTPUT 714;"STATUS:OPERATION:NMRREADY:ENABLE 16" !Sets New Measurement Results
!Ready Enable Regigter
!for bit 4
OUTPUT 714;"STATUS:OPERATION:NMRREADY:NTR 2" !Sets the New Measurement Results
!Ready Negative Transition Filter
!Register for bit 1
OUTPUT 714;"STATUS:OPERATION:NMRREADY:PTR 4" !Sets the New Measurement
!Results Ready Positive
!Transition Filter Register
!for bit 2
STATus:OPERation:NMRReady:AMPS Condition Register Bit Assignment
The STATus:OPERation:NMRReady:AMPS register bits indicate when a measurement has been completed and new measurement results are available.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
Reserved for future use.
|
This bit is always 0.
|
10
|
1024
|
Reserved for future use.
|
This bit is always 0.
|
9
|
512
|
Reserved for future use.
|
This bit is always 0.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
Reserved for future use.
|
This bit is always 0.
|
6
|
64
|
Reserved for future use.
|
This bit is always 0.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
Reserved for future use.
|
This bit is always 0.
|
3
|
8
|
Frequency Modulation New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States.
|
2
|
4
|
Frequency Stability New Measurement Result Ready
|
This is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States.
|
1
|
2
|
Analog Transmit Power New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States.
|
0
|
1
|
Extension Bit
|
This bit is always 0.
|
Program Examples - STATus:OPERation:NMRReady:AMPS
OUTPUT 714;"STATUS:OPERATION:NMRREADY:AMPS:EVENT?" !Queries the New Measurement
!Results Ready AMPS Event Register.
OUTPUT 714;"STATUS:OPERATION:NMRREADY:AMPS:CONDITION?" !Queries the New Measurement
!Results Ready AMPS
!Condition Register.
OUTPUT 714;"STATUS:OPERATION:NMRREADY:AMPS:ENABLE 8" !Sets New Measurement Results
!Ready AMPS Enable Register
!for bit 3.
OUTPUT 714;"STATUS:OPERATION:NMRREADY:AMPS:NTR 2" !Sets the New Measurement Results
!Ready AMPS Negative Transition
!Register for bit 1.
OUTPUT 714;"STATUS:OPERATION:NMRREADY:AMPS:PTR 4" !Sets the New Measurement
!Results Ready AMPS Positive
!Transition Register
!for bit 2.
STATus:OPERation:NMRReady:COMMon Condition Register Bit Assignment
The STATus:OPERation:NMRReady:COMMon register bits indicate when a measurement has been completed and new measurement results are available.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
Reserved for future use.
|
This bit is always 0.
|
11
|
2048
|
Reserved for future use.
|
This bit is always 0.
|
10
|
1024
|
Reserved for future use.
|
This bit is always 0.
|
9
|
512
|
Reserved for future use.
|
This bit is always 0.
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
Reserved for future use.
|
This bit is always 0.
|
6
|
64
|
Phase and Amplitude vs. Time |
This is the summary bit for the STATus:OPERation:NMRReady:COMMon Phase and Amplitude vs. Time register.
|
5
|
32
|
Frequency Stability
|
This is the summary bit for the STATus:OPERation:NMRReady:COMMon Frequency Stability register.
|
4
|
16
|
Multi-Tone Audio |
This is the summary bit for the STATus:OPERation:NMRReady:COMMon Multi-Tone Audio register.
|
3
|
8
|
Spectrum Monitor
|
This is the summary bit for the STATus:OPERation:NMRReady:COMMon Spectrum Monitor register.
|
2
|
4
|
Swept Audio |
This is the summary bit for the STATus:OPERation:NMRReady:COMMon Swept Audio register.
|
1
|
2
|
Audio Analyzer
|
This is the summary bit for the STATus:OPERation:NMRReady:COMMon Audio Analyzer register.
|
0
|
1
|
Extension Bit |
This bit is always 0.
|
Program Examples - STATus:OPERation:NMRReady:COMMon
OUTPUT 714;"STATUS:OPERATION:NMRREADY:COMMON:EVENT?" !Queries and clears the Operation
!New Measurement Results Ready
!Common Event Register
OUTPUT 714;"STATUS:OPERATION:NMRREADY:COMMON:CONDITION?" !Queries and clears the Operation
!New Measurement Results Ready
!Common Condition Register
OUTPUT 714;"STATUS:OPERATION:NMRREADY:COMMON:ENABLE 1024" !Sets the Operation
!New Measurement Results Ready
!Common Enable
!Register for bit 10
OUTPUT 714;"STATUS:OPERATION:NMRREADY:COMMON:NTRANSITION 2" !Sets the Operation
!New Measurement Results Ready
!Common Negative Transition
!Filter Register for bit 1
OUTPUT 714;"STATUS:OPERATION:NMRREADY:COMMON:PTRANSITION 2" !Set the Operation
!New Measurement Results Ready
!Common Positive Tranasition
!Filter Register for bit 1
STATus:OPERation:NMRReady:GPRS Condition Register Bit Assignment
The STATus:OPERation:NMRReady:GPRS register bits indicate when a GPRS measurement has been completed and new measurement results are available.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
EMACcuracy New Measurement Result Ready. |
|
13
|
8192
|
ETXPower New Measurement Result Ready.
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
12
|
4096
|
BLERror New Measurement Result Ready.
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
11
|
2048
|
GBERror New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
10
|
1024
|
DPOWer New Measurement Result Ready |
|
9
|
512
|
I/Q Tuning New Measurement Result Ready |
|
8
|
256
|
Reserved for future use.
|
This bit is always 0.
|
7
|
128
|
SBERror New Measurement Result Ready.
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
6
|
64
|
Reserved for future use.
|
This bit is always 0.
|
5
|
32
|
Reserved for future use.
|
This bit is always 0.
|
4
|
16
|
ORFSpectrum New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
3
|
8
|
PFERror New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
2
|
4
|
PVTime New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
1
|
2
|
TXPower New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
0
|
1
|
Extension Bit
|
This bit is always 0.
|
Program Examples - STATus:OPERation:NMRReady:GPRS
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GPRS:EVENT?" !Queries and clears the Operation
!New Measurement Results Ready
!GPRS Event Register
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GPRS:CONDITION?" !Queries and clears the Operation
!New Measurement Results Ready
!GPRS Condition Register
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GPRS:ENABLE 1024" !Sets the Operation
!New Measurement Results Ready
!GPRS Enable
!Register for bit 10
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GPRS:NTRANSITION 2" !Sets the Operation
!New Measurement Results Ready
!GPRS Negative Transition
!Filter Register for bit 1
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GPRS:PTRANSITION 2" !Sets the Operation
!New Measurement Results Ready
!GPRS Positive Tranasition
!Filter Register for bit 1
STATus:OPERation:NMRReady:GSM Condition Register Bit Assignment
The STATus:OPERation:NMRReady:GSM register bits indicate when a GSM measurement has been completed and new measurement results are available.
Bit Number
|
Binary Weighting
|
Condition
|
Description
|
15
|
32768
|
Not Used. Defined by SCPI.
|
This bit is always 0.
|
14
|
16384
|
Reserved for future use.
|
This bit is always 0.
|
13
|
8192
|
Reserved for future use.
|
This bit is always 0.
|
12
|
4096
|
FACCH Frame Erasure Rate (FER) New Measurement Result Ready. |
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
11
|
2048
|
Bad Frame Indication (BFI) New Measurement Result Ready. |
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
10
|
1024
|
DPOWer New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
9
|
512
|
I/Q Tuning New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
8
|
256
|
BERRor New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
7
|
128
|
FBERror New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
6
|
64
|
DAUDio New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
5
|
32
|
AAUDio New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
4
|
16
|
ORFSpectrum New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
3
|
8
|
PFERror New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
2
|
4
|
PVTime New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
1
|
2
|
TXPower New Measurement Result Ready
|
This bit is a 1 if the measurement has been completed and has produced new results.
This bit is a zero at power on, after a preset and while a measurement is in Measuring States. See
Triggering of Measurements
.
|
0
|
1
|
Extension Bit
|
This bit is always 0.
|
Program Examples - STATus:OPERation:NMRReady:GSM
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GSM:EVENT?" !Queries and clears the Operation
!New Measurement Results Ready
!GSM Event Register
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GSM:CONDITION?" !Queries and clears the Operation
!New Measurement Results Ready
!GSM Condition Register
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GSM:ENABLE 1024" !Sets the Operation
!New Measurement Results Ready
!GSM Enable
!Register for bit 10
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GSM:NTRANSITION 2" !Sets the Operation
!New Measurement Results Ready
!GSM Negative Transition
!Filter Register for bit 1
OUTPUT 714;"STATUS:OPERATION:NMRREADY:GSM:PTRANSITION 2" !Sets the Operation
!New Measurement Results Ready
!GSM Positive Tranasition
!Filter Register for bit 1