Last updated: December 3, 2008
Set/queries whether the audio generator signal or the FM demodulation signal is selected to be routed to the AUDIO OUT port of the test set's front panel. When audio generator is selected for output at the front-panel AUDIO OUT port, use AFGenerator Subsystem to control the audio generator.
|
||||||
GPRS TA | ||||||
EGPRS TA | ||||||
OUTPUT 714;"SYSTem:AUDio:OUTPut:SOURce FMDemod" ! Selects FM Demod signal for output at the front panel AUDIO OUT port. |
Sets/queries whether the fixed bandpass filter is inserted or bypassed in the FM Demod signal path. It is useful only when FM Demod signal is selected for output at the front-panel AUDIO OUT port (see SYSTem:AUDio:OUTPut:SOURce ). When the state is ON, a 300 Hz to 3 KHz bandpass filter is inserted in the audio signal path. When the state is OFF, the bandpass filter is bypassed in the audio signal path |
||
GPRS TA | ||
EGPRS TA | ||
Setting | Range: 0|OFF|1|ON | |
*RST setting | 0 (OFF) | |
OUTPUT 714;"SYSTem:AUDio:OUTPut:FMDemod:BPFilter:STATe ON" ! Sets the bandpass filter state to ON. |
Sets/queries whether the expandor filter is inserted or bypassed in the FM Demod signal path. It is useful only when FM Demod signal is selected for output at the front-panel AUDIO OUT port (see SYSTem:AUDio:OUTPut:SOURce ). When the state is ON, the expandor filter is inserted in the audio signal path. When the state is OFF, the expandor filter is bypassed in the audio signal path. |
||
GPRS TA | ||
EGPRS TA | ||
Setting | Range: 0|OFF|1|ON | |
*RST setting | 0 (OFF) | |
OUTPUT 714;"SYSTem:AUDio:OUTPut:FMDemod:EXPandor:STATe ON" ! Sets the expandor filter state to ON. |
Sets/queries whether the deemphasis filter is inserted or bypassed in the FM Demod signal path. It is useful only when FM Demod signal is selected for output at the front-panel AUDIO OUT port (see SYSTem:AUDio:OUTPut:SOURce ). When the state is ON, the deemphasis filter is inserted in the audio signal path. When the state is OFF, the deemphasis filter is bypassed in the audio signal path. |
||
GPRS TA | ||
EGPRS TA | ||
Setting | Range: 0|OFF|1|ON | |
*RST setting | 0 (OFF) | |
OUTPUT 714;"SYSTem:AUDio:OUTPut:FMDemod:DEEMphasis:STATe ON" ! Sets the deemphasis filter state to ON. |