Last updated: December 3, 2008
Queries the manufacturer, model number, model number of the test application running, serial number, revision, board ID, and cal file information. The information provided by the query represents the configuration that existed when the test set was powered up. For an example of how to use this command, see Hardware Configuration Report . |
||
GPRS TA | ||
EGPRS TA | ||
Requirements | ||
Resets have no effect on this information. The information is gathered during the power up cycle. |