SYSTem:CURRent:TA
Last updated: December 3, 2008
GPIB Command Conventions
SYSTem:CURRent:TA:MODel?
Function
|
GSM TA
|
Queries the model number of the test application running. Printable ASCII characters up to a 15 character string.
|
GPRS TA |
EGPRS TA |
GSM/GPRS LA
|
EGPRS LA
|
Query
|
Range: ASCII codes 32 - 126 decimal excluding comma and semicolon
|
*RST Setting
|
non volatile, read from the test set's hard disk
|
Requirements |
GSM/GPRS/
EGPRS TA
|
Revision: A.01 and above
|
GSM/GPRS/
EGPRS LA
|
Revision: C.01 and above
|
SYSTem:CURRent:TA:NAME?
Function
|
GSM TA
|
Queries the name of the test application running. Printable ASCII characters up to a 25 character string. This is not the recommended command, see
SYSTem:APPLication
for the recommended command.
|
GPRS TA |
EGPRS TA |
GSM/GPRS LA
|
EGPRS LA
|
Query
|
Range: ASCII codes 32 - 126 decimal excluding comma and semicolon
|
*RST Setting
|
non volatile, read from the test set's hard disk
|
Requirements |
GSM/GPRS/
EGPRS TA
|
Revision: A.01 and above
|
GSM/GPRS/
EGPRS LA
|
Revision: C.01 and above
|
SYSTem:CURRent:TA:REVision?
Function
|
GSM TA
|
Queries the coordinated codeware revision for the test application running. Printable ASCII characters up to a 20 character string. This is not the recommended command, see
SYSTem:APPLication
for the recommended command.
|
GPRS TA |
EGPRS TA |
GSM/GPRS LA
|
EGPRS LA
|
Query
|
Range: ASCII codes 32 - 126 decimal excluding comma and semicolon
|
*RST Setting
|
non volatile, read from the test set's hard disk. |
Requirements |
GSM/GPRS/
EGPRS TA
|
Revision: A.01 and above
|
GSM/GPRS/
EGPRS LA
|
Revision: C.01 and above
|