This command sets/queries the state of the Restart on Fatal Error parameter. See Restart on Fatal Error for more information. Error messages that are created when a fatal error occurs are entered in the error/event queue that can be queried with the command SYSTem:ERRor? . This is a nonvolatile setting, that is the instrument does not require a power supply to retain the setting its memory. |
|
0 | |
OUTPUT 714;"SYSTem:FATal:ERRor:RESTart ON" ! Commands the instrument to restart if a fatal error occurs. |