SYSTem:ROSCillator

SYSTem:ROSCillator

Last updated: December 3, 2008

GPIB Command Conventions

SYSTem:ROSCillator[:TIMebase]?

Function

GSM TA

Query to indicate if the test set's internal source or a suitable external source has been chosen to drive the test set's time base.

A suitable external source must have:

  • an output level of 0 to +13DBM
  • frequency of 10 MHZ
GPRS TA
EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Range:

  • INT = internal source
  • EXT = external source
Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/
EGPRS LA

Revision: C.01 and above

SYSTem:ROSCillator:LOCKed?

Function

GSM TA

Query the status of the reference oscillator and indicate if it is locked or unlocked.
GPRS TA
EGPRS TA

GSM/GPRS LA

EGPRS LA

Query

Range:

  • 0 = unlocked
  • 1 = locked
Requirements

GSM/GPRS/
EGPRS TA

Revision: A.01 and above

GSM/GPRS/
EGPRS LA

Revision: C.01 and above