Frequency Offset

Frequency Offset

Last updated: September 1, 2009

The random frequency offset functionality allows you to set a fixed or random frequency offset to the carrier. You can specify one of the following three frequency offset modes:

Note that a large frequency offset value may cause a failure in call establishment process.

The GPIB command to set Frequency Offset Mode is CALL[:CELL]:FOFFset:[Mode]

The GPIB command to specify the value of the frequency offset is CALL[:CELL]:FOFFset:VALue

See How Do I Change Cell Operation Parameters? to access to this setting.

Related Topics


CALL:FOFFset

Downlink Dual Carrier