SETup:TSEMask

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions.

For the measurement, see Spectrum Emission Mask (SEM) Measurement.

SETup:TSEMask:CONTinuous

Function

Sets/queries the trigger arm state for the Spectrum Emission Mask measurement.

The trigger arm state determines whether the measurement will be made once then stop (0|OFF (single)) or automatically re-arm upon completion of one measurement and repeat the process (1|ON (continuous)).

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0(Off)

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETUP:TSEMASK:CONTINUOUS OFF"

SETup:TSEMask:COUNt[:SNUMber]

Function

Sets/queries the number of the Spectrum Emission Mask  measurement to be made in a multi-measurement setup.

This command sets the count, and automatically sets the multi-measurement STATe command to 1 (on).

Setting

Range: 1 to 999

Query

Range: 1 to 999

*RST Setting

Off (10 when STATe = On)

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETup:TSEMask:COUNt:SNUMber 5"

SETup:TSEMask:COUNt:NUMBer

Function

Sets/queries the number of the Spectrum Emission Mask measurement to be made when multi-measurement state is ON:

Setting

Range: 1 to 999

Query

Range: 1 to 999

*RST Setting

10

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETup:TSEMask:COUNt:NUMber 5"

SETup:TSEMask:COUNt:STATe

Function

Sets/queries the multi-measurement state of Spectrum Emission Mask measurement.

Setting

Range: 1|ON|0|OFF

Query

Range:1|0

*RST Setting

0 (off)

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETUP:TSEMask:COUNT:STATE ON"

SETup:TSEMask:LIMit

Function

Sets/queries the pass/fail limits for the following frequency offsets in the Spectrum Emission Mask measurement:

  • 30 kHz filter ±0.8 MHz

  • 30 kHz filter ±1.8 MHz  

  • 30 kHz filter ±2.4 MHz  

  • 1 MHz filter ±2.4 MHz

  • 1 MHz filter ±4.0 MHz

Setting

Range:-80 to 10 dBc

Query

Range:-80 to 10 dBc

*RST Setting

  • 30 kHz filter ±0.8 MHz: -35.0 dBc

  • 30 kHz filter ±1.8 MHz: -49.0 dBc

  • 30 kHz filter ±2.4 MHz: -59.2 dBc

  • 1 MHz filter ±2.4 MHz: -44.0 dBc

  • 1 MHz filter ±4.0 MHz: -44.0 dBc

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETup:TSEMask:LIMit -35,-49,-59,-44,-44"

SETup:TSEMask:POWer:RANGe:OFFSet:MANual

Function

Sets/queries the value of Manual Power Range Offset.

Setting

Range:-25dB to 25dB

Resolution: 0.01 dB

Unit: dB

Query

Range:-25dB to 25dB

*RST Setting

0.00dB

Requirements

Test Application Revision:  A.06.00 and above

Programming Example

"SETup:TSEMask:POWer:RANGe:OFFSet:MANual 6dB"

SETup:TSEMask:TIMeout[:STIMe]

Function

 (1) sets the Spectrum Emission Mask measurement's timeout value, (2) sets the  measurement's timeout STATe to 1 (on)

Setting

Range: 0.1 to 999.9 seconds

Resolution: 0.1 second

Query

Range: 0.1 to 999.9 seconds

*RST Setting

10 seconds,off

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETup:TSEMask:TIMeout:STIMe 5 S"

SETup:TSEMask:TIMeout:TIME

Function

Sets/queries the Spectrum Emission Mask measurement's timeout  setting to be used when the timeout state is set to ON.

Setting

Range: 0.1 to 999.9 seconds

Resolution: 0.1 second

Query

Range: 0.1 to 999.9 seconds

*RST Setting

10 seconds

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETup:TSEMask:TIMeout:TIMe 5 S"

SETup:TSEMask:TRIGger:SOURce

Function

Sets/queries the Trigger Source of the Spectrum Emission Mask measurement.

Setting

Range:AUTO | IMMediate | RISE | EXTernal | PROTocol

Query

Range:AUTO | IMM | RISE | EXT | PROT

*RST Setting

AUTO

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETup:TSEMask:TRIGger:SOURce IMMEDIATE"

SETup:TSEMask:TRIGger:DELay

Function

Sets/queries the Trigger Delay setting of the Spectrum Emission Mask measurement:

This setting can be used to delay the measurement trigger in order to start a measurement during a specific timeslot in the frame.

Setting

Range: -10 to 10 ms

Resolution: 0.1 us

Query

Range: -10 to 10 ms

Resolution: 0.1 us

*RST Setting

0ms

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SETup:TSEMask:TRIGger:DELay 1MS"

SETup:TSEMask:TSLot:MEASure

Function

Sets/queries which uplink time slot to be measured.

Setting

Range: TS1 | TS2 | TS3 |TS4

Query

Same as setting

*RST Setting

TS1

Requirements

Test Application Revision:  A.06.00 and above

Programming Example

"SETup:TSEMask:TSLot:MEASure TS1"