Time Slot to Measure

Last updated: 2014-11-28

Time Slot to Measure Description

Through the Time Slot to Measure setting, you can select which uplink time slot the test set will measure. This setting has been applied to four measurements:  Adjacent Channel Leakage Ratio (ACLR) Measurement, Channel Power Measurement, Spectrum Emission Mask (SEM) Measurement, and Waveform Quality Measurement.

Time Slot to Measure Parameters

There are four parameters: TS1, TS2, TS3, and TS4.

The default setting is TS1.

Time Slot to Measure Requirements

The operating mode is set to Active Cell.

          Or else, this setting will be out of scope and won't affect the measurement behavior.

          When the setting is in scope and takes effect, the trigger delay will act alongside this setting.

Related Topics

GPIB Command: SETup:TCPower:TSLot:MEASure

                            SETup:TACLeakage:TSLot:MEASure

                            SETup:TSEMask:TSLot:MEASure

                            SETup:TWQuality:TSLot:MEASure