Trigger Output Setup

Trigger Output Setup

Last updated: January 15, 2009

The test set provides a 5 V, 16.5 us pulse at the TRIG OUT rear panel connector for triggering other test equipment from the test set.

This pulse is generated according to the Trigger Output Setup setting:

To access Trigger Output Setup from the front panel, press the CALL SETUP key, press the More key until you reach the Call Control 2 of 5 menu, and then select Trig Output Setup ( F6 ).

Related Topics


CALL:TRIGger

Rear Panel Connectors