How Do I Make a Loopback Bit Error Ratio (BER) Measurement?

How Do I Make a Loopback Bit Error Ratio (BER) Measurement?

Last updated: January 15, 2009

Measuring Loopback Bit Error Ratio

  1. Press the Measurement selection key.
  2. Select the Loopback Bit Error Ratio measurement.
  3. Select Bit Error Setup ( F1 ).

    Select Close Menu ( F6 ).

  4. Establish an RB Test Mode connection between the UE and test set (see How Do I Set Up a Call and Make a Connection? ).
  5. Set UE Target Power to +21 dBm (for a Power Class 4 UE).
  6. Set Cell Power ( F7 ) to -106 dBm (for Operating Band I).
  7. Press the START SINGLE key to begin the measurement.
  8. If the Confidence Test Result is Max Bits Tested , start the measurement again. You may need to increase the Number of Bits to Test to enable a Pass or Fail result.
  9. Adjust Cell Power ( F7 ), AWGN Power ( F4 ), Soft Handover ( F3 ) and Cell 2 Power ( F2 ) as desired.

An example measurement result is shown below:

Related Topics


Loopback Bit Error Ratio (BER) Measurement Description

Loopback Bit Error Ratio Troubleshooting

Programming a Loopback Bit Error Ratio Measurement