How Do I Change Receiver Control Parameters?

How Do I Change Receiver Control Parameters?

Last updated: January 15, 2009

In some instances you may want to control the test set's receiver settings manually rather than allowing the test set to automatically control them. This ability is referred to as manual receiver control (see Receiver Control ).

Manual Receiver Control in Active Cell, Cell Off or FDD Test Operating Mode

  1. Press the CALL SETUP key.
  2. Press Operating Mode ( F1 ) and select Active Cell, or Cell Off, or FDD Test .
  3. Press the More key two times until 3 of 3 is displayed.
  4. Press the Receiver Control ( F12 ) key.
  5. To manually set the receiver's expected power, highlight the Power Control field and select Manual , then enter a a desired value in the Manual Power field by using the knob or numeric keys.
  6. To manually set the receiver's measurement downconverter frequency, highlight the Measurement Frequency field and enter a desired value to replace the Auto with the knob or numeric keys.
  7. (In FDD Test mode only) To manually set the receiver's demodulation downconverter tune frequency, turn the knob to highlight the Uplink Frequency field and enter a desired value to replace the Auto with the knob or numeric keys.

Manual Receiver Control in CW Operating Mode

  1. Press the CALL SETUP key.
  2. Press Operating Mode ( F1 ) and select CW .
  3. Press the Receiver Control ( F12 ) key.
  4. To set the receiver's expected power, turn the knob to highlight the Expected CW Power field and press the knob, then enter a desired value by using the knob or numeric keys and press the knob.
  5. To set the measurement downconverter's tune frequency, turn the knob to highlight the Measurement Frequency field and press the knob, then enter a desired value by using the knob or numeric keys and press the knob.
  6. To set the demodulation downconverter's tune frequency, turn the knob to highlight the Uplink Frequency field and press the knob, then enter a desired value by using the knob or numeric keys and press the knob.
  7. Press Close Menu ( F6 ).

Related Topics


Receiver Control

Active Cell Operating Mode

CW Operating Mode