Last updated: January 16, 2009
Audio Frequency measures the frequency of the signal applied to the front-panel AUDIO IN connectors, and is one of the Audio Analyzer measurements. Audio frequency can be measured for signals in the frequency range of 100 Hz to 15 kHz, at levels from 7.1 mV peak to 20V peak, and with a signal-to-noise ratio of 30 dB or greater.
The audio frequency measurement is made after any filtering and processing are selected for the Audio Analyzer.