IQ Tuning Measurement Description

IQ Tuning Measurement Description

Last updated: January 16, 2009

How is an IQ Tuning Measurement Made?

The IQ tuning measurement includes all of the measurements available in the Waveform Quality measurement (see Waveform Quality Measurement Results ), along with the following measurement results:

Measurement Interval in Non-HSDPA Mode

When on a non-HSDPA connection, you must set Trigger Source to any value other than HS-DPCCH . When operating in this mode, the measurement is made during one timeslot (666.7 us). You can choose in which timeslot of the W-CDMA frame the measurement is performed using the Timeslot setting.

Timeslot Setting

Measurement Interval in HSDPA Mode

This section is only applicable to the lab application or feature-licensed test application .

To measure IQ tuning on an HSDPA connection, you must set Trigger Source to HS-DPCCH . When Trigger Source is set to HS-DPCCH, you can specify the measurement interval and its placement within any of the 6 HSDPA subframes.

  1. Use the HS-DPCCH Trigger Subframe Alignment setting to choose in which 2 ms subframe (0 to 5) you want to place the measurement interval.
  2. Use the HS-DPCCH Trigger Slot Alignment setting to specify in which slot within the subframe you want to place the measurement interval ( AckNack = the first slot of the subframe, CQI1 = the second slot of the subframe and CQI2 = the third slot of the subframe).
  3. Set the duration of the measurement interval using the HS-DPCCH Measurement Interval setting. Note that the sum of HS-DPCCH Trigger Subslot Alignment and HS-DPCCH Measurement Interval cannot exceed 1.0 slot.
  4. Use the HS-DPCCH Trigger Subslot Alignment setting to specify where you want to place the measurement interval within the slot. You can place the measurement interval at the slot boundary, 0.1 slot (66.7 us) after the slot boundary, 0.2 slot (133.3 us) after the slot boundary... up to 0.5 slot (333.3 us) after the slot boundary. Note, however, that the sum of HS-DPCCH Trigger Subslot Alignment and HS-DPCCH Measurement Interval cannot exceed 1.0 slot. If you wish to place the measurement interval after the slot boundary using the HS-DPCCH Trigger Subslot Alignment setting, you must first decrease the HS-DPCCH Measurement Interval setting appropriately.
  5. You can choose to shorten the measurement interval so as to exclude the 25 us (96 chip) transient periods at the start and end of the measurement interval using the Transient Period setting. For example, if you set HS-DPCCH Measurement Interval to 0.5 slot (333.3 us or 1280 chips) and set Transient Period to Exclude , the measurement is performed over 283.3 us (or 1088 chips).

Measurement Interval Duration and Placement for HSDPA

IQ Tuning Measurement Parameters

HSDPA Measurement Parameters

This section is only applicable to the lab application or feature-licensed test application .

These settings are only applicable when Trigger Source = HS-DPCCH .

See Measurement Interval in HSDPA Mode for more information about using these parameters to specify the duration and placement of the measurement interval.

IQ Tuning Measurement Results

Chip EVM and the IQ constellation are graphed together on the same screen. See figure IQ Tuning Graph Display for an example display. You can use the Axis Control ( F2 ) and the Marker ( F3 ) settings to control the Chip EVM trace graph and the IQ constellation diagram. The IQ constellation diagram is always redrawn to reflect the latest Chip EVM settings. For example, if the chip EVM for chips 512 through 1023 are plotted, then the IQ constellation is shown for just chips 512 through 1023. The I and Q values for the IQ constellation all range between -1.0 and +1.0.

IQ Tuning Graph Display

The IQ tuning measurement also returns all of the measurement results of the Waveform Quality measurement. Waveform Quality Measurement Results

IQ Tuning Input Signal Requirements

IQ Tuning Measurement Calibration

This measurement should be calibrated using the Calibrate Measurements function ( CALibration:MEASurements? ) when the temperature has changed by ± 10° C or more since the last calibration. If this situation exists, the integrity indicator value becomes 19 and a message is displayed indicating "Uncalibrated Due to Temperature".

Related Topics