Change of TFC (Transport Format Combination) Measurement Description

Change of TFC (Transport Format Combination) Measurement Description

Last updated: January 16, 2009

This section is only applicable to the lab application.

How is a Change of TFC Measurement Made?

When a UE changes its TFC, it must change its output power in accordance with any resulting change in data rate. The 3GPP TS 34.121 5.6 Change of TFC test addresses the case of an uplink 12.2k RMC operating in DTX (Discontinuous Transmission) mode, wherein the DPDCH is periodically turned off. The test confirms that the UE's output power level changes properly when its DPDCH is turned off.

The change of TFC measurement requires an RB Test Mode connection between the test set and UE, in either loopback mode 1 or 2. When the measurement is initiated, the test set stops sending a constant stream of data (to be looped back by the UE), and instead sends a block of data, then a block of no data, repeatedly. This causes the UE to turn its DPDCH on and off on a block-by-block basis. The test set monitors the uplink TFCI and the change of TFC measurement is triggered when the TFCI indicates no data is present on the DPDCH (the DPDCH is thus off for that block). The test set then measures the mean power in the timeslot before and after the transition from DPDCH on to DPDCH off, and before and after the transition from DPDCH off to DPDCH on. The power measurements do not include the transient periods of 25 us on either side of the timeslot boundaries. Thus, the measurement interval is 2368 chips, or 617 us. The measurement then reports the step change in power ( P as described in 3GPP TS 34.121 5.6) for both transitions (see Step Down Relative Power (in dB) and Step Up Relative Power (in dB) ).

3GPP TS 34.121 5.6.2 Transmit template during DTX

Required Initial Conditions

Before performing the change of TFC measurement, you must:

Recommended Initial Conditions

The following settings are recommended based on the 3GPP TS 34.121 5.6 requirements:

No other measurements can be running when a change of TFC measurement is performed. If any measurements are running when a change of TFC measurement is initiated, they are closed and a message is displayed to indicate that they were closed. Likewise, if any other measurements are initiated while a change of TFC measurement is running, the change of TFC measurement is closed and a message is displayed.

Change of TFC Measurement Parameters

The following four parameters can be independently set for the 12.2k RMC, 33k No Coding RMC, 64k RMC, 144k RMC and 384k RMCs:

Change of TFC Measurement Results

Change of TFC Measurement Input Signal Requirements

Change of TFC Measurement Calibration

You must calibrate this measurement using the measurement calibration procedure (see Calibrating the Test Set ).

Related Topics

Manual Operation: How Do I Make a Change of TFC (Transport Format Combination) Measurement?

Programming a Change of TFC (Transport Format Combination) Measurement

Change of TFC (Transport Format Combination) Troubleshooting

What 3GPP W-CDMA/HSPA Conformance Tests Are Supported?

Triggering of Measurements

Integrity Indicator