This section describes the BURSt subsystem.
This summarizes the steps required to generate a burst.
The following code produces the oscilloscope image shown below.
APPLy:SIN 1e5,3 VPP,0
BURS:MODE TRIG
BURS:NCYC 3
BURS:INT:PER 4.4e-5
BURS:PHAS 0
TRIG:SOUR IMM
BURS:STAT ON
OUTP 1
There are two burst modes, described below. The instrument enables one burst mode at a time.
The following table shows which modes are associated with which burst features.
Burst Mode
BURSt:MODE |
Burst Count
BURSt:NCYCles |
Burst Period
BURSt:INTernal:PERiod |
Burst Phase
BURSt:PHASe |
Trigger Source
TRIGger[1|2]:SOURce |
|
Triggered Burst Mode:
|
TRIGgered | Available | Available | Available | IMMediate |
Triggered Burst Mode:
External Trigger |
TRIGgered | Available | Not Used | Available | EXTernal, BUS |
Gated Burst Mode:
|
GATed | Not Used | Not Used | Available | Not Used |
The difference between gated burst and gated output is that gated burst synchronously starts and stops using full waveform cycles, where gated output asynchronously turns instrument output on or off with an external trigger, independent of the waveform phase.
If the duty cycle is changed on a triggered bursted square wave with the trigger mode set to Timer, the current burst will finish and one more burst will be executed before the duty cycle of the burst changes. |
Selects true-high (NORMal) or true-low (INVerted) logic levels on the rear-panel Ext Trig connector for an externally gated burst.
Parameter | Typical Return |
---|---|
{NORMal|INVerted}, default NORMal | NORM or INV |
Select true-low logic for an externally gated burst: BURS:GATE:POL INV |
Sets the burst period for internally-triggered bursts.
Parameter | Typical Return |
---|---|
1 µs to 8000 s, default 10 ms | +1.200000000000000E+01 |
Sets the burst period to 12 seconds: BURS:INT:PER 12 |
Selects the burst mode.
Parameter | Typical Return |
---|---|
{TRIGgered|GATed}, default TRIGgered | TRIG or GAT |
Set gated burst mode BURS:MODE GATED |
Sets the number of cycles to be output per burst (triggered burst mode only).
Parameter | Typical Return |
---|---|
Whole number from 1 (default) to 100,000,000, limited as described below |
+5.000000000000000E+01 |
Return number of cycles per burst: BURS:NCYC 50 |
Sets the starting phase angle for the burst.
Parameter | Typical Return |
---|---|
-360 to +360 degrees, -2p to +2p radians, or -(period) to +(period), as specified by UNIT:ANGLe. Default 0. |
+6.0000000000000E+01 |
Set starting burst phase to 60 degrees: UNIT:ANGLE DEG BURS:PHAS 60 |
Enables or disables burst mode.
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}, default OFF |
0 (OFF) or 1 (ON) |
Enable burst mode: BURS:STAT ON |