The OUTPut subsystem controls the front panel channel output and Sync connectors and the rear-panel Ext Trig connector:
Enables or disables the front panel output connector.
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}, default OFF | 0 (OFF) or 1 (ON) |
Enable output connector for channel 1: OUTP ON |
Sets expected output termination. Should equal the load impedance attached to the output.
Parameter | Typical Return |
---|---|
1 Ω to 10 kΩ, default 50 Ω | +5.000000000000000E+02 |
Set output impedance to 300 Ω: Set output impedance to "high impedance": |
Enables (GATed) or disables (NORMal) gating of the output waveform signal on and off using the trigger input.
Parameter | Typical Return |
---|---|
{NORMal|GATed}, default NORMal | GAT or NORM |
Enable gated output: |
Inverts waveform relative to the offset voltage.
Parameter | Typical Return |
---|---|
{NORMal|INVerted}, default NORMal | NORM or INV |
Set output polarity to INVerted: OUTP:POL INV |
Disables or enables the front panel Sync connector.
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}, default ON | 0 (OFF) or 1 (ON) |
Disable front panel Sync connector: OUTP:SYNC OFF |
Specifies normal Sync behavior (NORMal), forces Sync to follow the carrier waveform (CARRier), or indicates marker position (MARKer).
Parameter | Typical Return |
---|---|
{NORMal|CARRier|MARKer}, default NORMal | NORM, CARR, or MARK |
Set output sync mode to CARRier: OUTPut:SYNC:MODE CARR |
<mode> | Sync Behavior | Conditions |
---|---|---|
NORMal | Sync follows envelope of burst signal. | When BURSt is on |
Sync follows envelope of sweep signal. | When SWEep is on | |
Sync follows modulating signal. | When modulating and modulation source is internal | |
Sync follows FUNC signal. | All other conditions | |
CARRier | Sync follows current SOURce:MARKer:POINt setting. | When BURSt or SWEep is on and FUNC is ARB |
Sync follows FUNC signal while burst is on. | When BURSt is on and FUNC is not ARB | |
Sync follows FUNC signal. | All other conditions | |
MARKer | Sync follows current SOURce:MARKer:POINt setting. | When in CW mode and FUNC is ARB When modulating, modulation source is internal, and FUNC is ARB or <modulation>:INT:FUNC is ARB When modulating, modulation source is external, and FUNC is ARB |
Sync follows current SOURce:MARKer:CYCLe setting. | When BURST is on | |
Sync follows current SOURce:MARKer:FREQuency setting. | When SWEEP is on | |
Sync follows modulating signal. | When modulating, modulation source is not external, FUNC is not ARB, and INT:FUNC is not ARB | |
Sync follows FUNC signal. | All other conditions |
Sets the desired output polarity of the Sync output to trigger external equipment that may require falling or rising edge triggers.
Parameter | Typical Return |
---|---|
{NORMal|INVerted}, default NORMal | NORM or INV |
Set the instrument's output sync connector to normal behavior: OUTP:SYNC:POL NORM |
Sets the source for the Sync output connector.
Parameter | Typical Return |
---|---|
{CH1|CH2}, default CH1 | CH1 or CH2 |
Set sync source to channel 2: OUTP :SYNC:SOUR CH2 |
Disables or enables the "trigger out" signal for sweep and burst modes.
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}, default OFF | 0 (OFF) or 1 (ON) |
Enable trigger out signal: OUTP:TRIG ON |
Selects whether the instrument uses the rising edge or falling edge for the "trigger out" signal.
Parameter | Typical Return |
---|---|
{POSitive|NEGative}, default POSitive | POS or NEG |
Set trigger slope to NEGative (falling edge): OUTP:TRIG:SLOP NEG |
Selects the source channel used by trigger output on a two-channel instrument. The source channel determines what output signal to generate on the trigger out connector.
Parameter | Typical Return |
---|---|
{CH1|CH2}, default CH1 | CH1 or CH2 |
Set output trigger source to CH2: OUTP:TRIG:SOUR CH2 |