The VOLTage subsystem sets parameters related to output voltage.
The following is a typical procedure using the VOLTage subsystem.
This example demonstrates the procedure outlined above:
SOURce1:FUNCtion SQU
SOURce1:FREQuency +1.0E+06
SOURce1:VOLTage +0.5
SOURce1:VOLTage:OFFSet +0.5
SOURce1:FUNCtion:SQUare:PERiod +1.0E-06
SOURce1:FUNCtion:PULSe:PERiod +1.0E-06
SOURce1:VOLTage:LIMit:LOW +0.0
SOURce1:VOLTage:LIMit:HIGH +1.0
SOURce1:VOLTage:LIMit:STATe 1
OUTP1 ON
SOURce2:FUNCtion SIN
SOURce2:FREQuency +1.0E+06
SOURce2:VOLTage +2.0
SOURce2:VOLTage:OFFSet +0.0
SOURce2:VOLTage:LIMit:LOW -1.0
SOURce2:VOLTage:LIMit:HIGH +1.0
SOURce2:VOLTage:LIMit:STATe 1
OUTP2 ON
Sets output amplitude.
Parameter | Typical Return |
---|---|
1 mVpp to maximum allowed for waveform and model, default 100 mVpp | +5.0000000000000E+00 |
Set output amplitude to 5 Vpp: VOLT 5 Vpp |
Use VOLTage:UNIT to specify output units for all subsequent commands.
You cannot specify output amplitude in dBm if output termination is set to high impedance. The units are automatically converted to Vpp.
Changing amplitude may briefly disrupt output at certain voltages due to output attenuator switching. The amplitude is controlled, however, so the output voltage will never exceed the current setting while switching ranges. To prevent this disruption, disable voltage autoranging using VOLTage:RANGe:AUTO OFF. The APPLy command automatically enables autoranging.
Enables or disables the maintaining of the same amplitude, offset, range, load, and units on both channels of a two-channel instrument. The command applies to both channels; the SOURce keyword is ignored.
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}, default OFF | 0 (OFF) or 1 (ON) |
Enable voltage coupling: VOLT:COUP ON |
Set the waveform's high and low voltage levels.
Parameter | Typical Return |
---|---|
±5 VDC into 50 Ω, as long as HIGH is at least 1 mV greater than LOW. Defaults: HIGH +50 mV, LOW -50 mV. | +4.000000000000000E+00 |
Set high voltage level to 4 V: VOLT:HIGH 4 |
Sets the high and low limits for output voltage.
Parameter | Typical Return |
---|---|
±5 VDC into 50 Ω, as long as HIGH is at least 1 mV greater than LOW. Defaults: HIGH +50 mV, LOW -50 mV. |
+5.0000000000000E+00 |
Set channel 1 output high limit to 5 V: VOLT:LIMIT:HIGH 5.0 VOLT:LIMIT:STATE ON |
Enables or disables output amplitude voltage limits.
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}, default OFF | 0 (OFF) or 1 (ON) |
Set and enable ±2.5 V output limits on channel 1: VOLT:LIM:HIGH 2.5 VOLT:LIM:LOW -2.5 VOLT:LIM:STAT ON |
Sets DC offset voltage.
Parameter | Typical Return |
---|---|
± 5 VDC into 50 Ω, default 0 | +1.0000000000000E-01 |
Set offset voltage to 100 mV: VOLT:OFFS 100 mV |
Changing amplitude may briefly disrupt output at certain voltages due to output attenuator switching. The amplitude is controlled, however, so the output voltage will never exceed the current setting while switching ranges. To prevent this disruption, disable voltage autoranging using VOLTage:RANGe:AUTO OFF. The APPLy command automatically enables autoranging.
Disables or enables voltage autoranging for all functions. Selecting ONCE performs an immediate autorange and then turns autoranging OFF
Parameter | Typical Return |
---|---|
{OFF|0|ON|1|ONCE}, default ON | 0 (OFF) or 1 (ON) |
Turn voltage autoranging OFF: VOLT:RANG:AUTO 0 |
Selects the units for output amplitude.
Parameter | Typical Return |
---|---|
{VPP|VRMS|DBM}, default VPP | VPP, VRMS, or DBM |
Set output amplitude units to Vrms: VOLT:UNIT VRMS |